LoftedFlangeBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
LoftedFlangeBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Lofted Flange feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateLoftedFlangeFeatureBuilder
Default values.
Property Value IndexMarkLength.Value 5 (millimeters part), 0.5 (inches part) NumberOfBendSegments 0 UseSegmentedBends 0 New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BendOptions | Returns the bend options object. |
EndSection | Returns or sets the end section of the lofted flange. |
EndSectionPoint | Returns or sets the start/end point of the end section. |
EndSketch | Returns or sets the end section sketch as slave. |
IndexMarkLength | Returns the index mark length Get the index mark length expression If use segmented bends is set to true the only the index mark length value is used for dividing the bend even though a value is set Index mark length value only gets reflected in flat pattern view |
IsSecondary | Returns or sets the type of lofted flange feature - base lofted flange/secondary lofted flange. |
NumberOfBendSegments | Returns or sets the number of bend segments Get and set the number of bend segments If use segmented bends is set to true then only the number of bend segments value is used for dividing the bend even though a value is set |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
StartSection | Returns or sets the start section of the lofted flange. |
StartSectionPoint | Returns or sets the start/end point of the start section. |
StartSketch | Returns or sets the start section sketch as slave. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ThicknessSide | Returns or sets the thickness side of base lofted flange. |
UseSegmentedBends | Returns or sets the use multi segment bends Set use_segmented_bends to true or false and get the same If use multi segment bends is set to true then lofted flange bend face is gets divided as per the number bend segments mentioned by the user |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetThickness | The thickness of base lofted flange. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetThickness | The thickness of base lofted flange. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify user data validity. |
Enumerations¶
LoftedFlangeBuilderSectionSideOptions Enumeration | This enum represents the side of the section that the lofted flange creates thickness. |
Property Detail¶
BendOptions¶
-
LoftedFlangeBuilder.
BendOptions
¶ Returns the bend options object.
Get the bend options object which is created while creating builder. Then set values to parameters of bend options object(like bend radius, bend relief type etc.) using set methods of bend options object.
-------------------------------------
Getter Method
Signature
BendOptions()
Returns: Return type: NXOpen.Features.SheetMetal.BendOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
EndSection¶
-
LoftedFlangeBuilder.
EndSection
¶ Returns or sets the end section of the lofted flange.
The section profile should be open looped.
-------------------------------------
Getter Method
Signature
EndSection()
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
EndSection(endSection)
Parameters: endSection ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
EndSectionPoint¶
-
LoftedFlangeBuilder.
EndSectionPoint
¶ Returns or sets the start/end point of the end section.
It can be start/end point of the section profile.
-------------------------------------
Getter Method
Signature
EndSectionPoint()
Returns: point Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
EndSectionPoint(point)
Parameters: point ( NXOpen.Point3d
) – pointNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
EndSketch¶
-
LoftedFlangeBuilder.
EndSketch
¶ Returns or sets the end section sketch as slave.
Set the sketch which is used to create end section. This is only used when the section is created from sketch. If the section is created from edges or if the end sketch is not required to be slave, set the value as None .
-------------------------------------
Getter Method
Signature
EndSketch()
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
EndSketch(slaveEndSketch)
Parameters: slaveEndSketch ( NXOpen.Features.SketchFeature
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
IndexMarkLength¶
-
LoftedFlangeBuilder.
IndexMarkLength
¶ Returns the index mark length Get the index mark length expression If use segmented bends is set to true the only the index mark length value is used for dividing the bend even though a value is set Index mark length value only gets reflected in flat pattern view
-------------------------------------
Getter Method
Signature
IndexMarkLength()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
IsSecondary¶
-
LoftedFlangeBuilder.
IsSecondary
¶ Returns or sets the type of lofted flange feature - base lofted flange/secondary lofted flange.
Specify false for base lofted flanges and true for secondary lofted flanges.
-------------------------------------
Getter Method
Signature
IsSecondary()
Returns: Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
IsSecondary(isSecondary)
Parameters: isSecondary (bool) – New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
NumberOfBendSegments¶
-
LoftedFlangeBuilder.
NumberOfBendSegments
¶ Returns or sets the number of bend segments Get and set the number of bend segments If use segmented bends is set to true then only the number of bend segments value is used for dividing the bend even though a value is set
-------------------------------------
Getter Method
Signature
NumberOfBendSegments()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfBendSegments(numberOfBendSegments)
Parameters: numberOfBendSegments (int) – New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
StartSection¶
-
LoftedFlangeBuilder.
StartSection
¶ Returns or sets the start section of the lofted flange.
The section profile should be open looped.
-------------------------------------
Getter Method
Signature
StartSection()
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
StartSection(startSection)
Parameters: startSection ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
StartSectionPoint¶
-
LoftedFlangeBuilder.
StartSectionPoint
¶ Returns or sets the start/end point of the start section.
It can be start/end point of the section profile.
-------------------------------------
Getter Method
Signature
StartSectionPoint()
Returns: point Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
StartSectionPoint(point)
Parameters: point ( NXOpen.Point3d
) – pointNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
StartSketch¶
-
LoftedFlangeBuilder.
StartSketch
¶ Returns or sets the start section sketch as slave.
Set the sketch which is used to create start section. This is only used when the section is created from sketch. If the section is created from edges or start sketch is not required to be slave, set slave sketch as None.
-------------------------------------
Getter Method
Signature
StartSketch()
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
StartSketch(slaveStartSketch)
Parameters: slaveStartSketch ( NXOpen.Features.SketchFeature
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ThicknessSide¶
-
LoftedFlangeBuilder.
ThicknessSide
¶ Returns or sets the thickness side of base lofted flange.
-------------------------------------
Getter Method
Signature
ThicknessSide()
Returns: Return type: NXOpen.Features.SheetMetal.LoftedFlangeBuilderSectionSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
ThicknessSide(thickSide)
Parameters: thickSide ( NXOpen.Features.SheetMetal.LoftedFlangeBuilderSectionSideOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
UseSegmentedBends¶
-
LoftedFlangeBuilder.
UseSegmentedBends
¶ Returns or sets the use multi segment bends Set use_segmented_bends to true or false and get the same If use multi segment bends is set to true then lofted flange bend face is gets divided as per the number bend segments mentioned by the user
-------------------------------------
Getter Method
Signature
UseSegmentedBends()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseSegmentedBends(useMultiSegmentBends)
Parameters: useMultiSegmentBends (bool) – New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
GetThickness¶
-
LoftedFlangeBuilder.
GetThickness
¶ The thickness of base lofted flange.
Applicable only for Base lofted flange. Ignored for a Secondary Lofted Flange.
Signature
GetThickness()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetThickness¶
-
LoftedFlangeBuilder.
SetThickness
¶ The thickness of base lofted flange.
Applicable only for Base lofted flange. Ignored for a Secondary Lofted Flange.
Signature
SetThickness(thickness)
Parameters: thickness (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
Expression.RightHandSide
on theExpression
object returned fromFeatures.SheetMetal.LoftedFlangeBuilder.GetThickness
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Validate¶
-
LoftedFlangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
LoftedFlangeBuilder.
ValidateBuilderData
¶ Verify user data validity.
If the data is valid, returned value should be 0.
Signature
ValidateBuilderData()
Returns: Data Validity Flag. Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)