MiterOptions Class¶
-
class
NXOpen.Features.SheetMetal.
MiterOptions
¶ Bases:
NXOpen.TaggedObject
Represents a Miter Data Options builder.
Mitre cut is essentially an end treatment to the contour flange feature, which shall prevent merging/interference with the existing or newly placed features in sheet metal. .. versionadded:: NX4.0.0
Properties¶
Property | Description |
---|---|
ClosedCornerType | Returns or sets the closed corner option type. |
ClosedCornerVAngle1 | Returns the v cutout angle1 expression of the closed corner. |
ClosedCornerVAngle2 | Returns the v cutout angle2 expression of the closed corner. |
EndType | Returns or sets the miter end type. |
MiterInteriorCornersIfNecessary | Returns or sets the miter_corners option. |
Position | Returns or sets the position of miter. |
StartType | Returns or sets the miter start type. |
Tag | Returns the Tag for this object. |
UseNormalCutoutMethod | Returns or sets the cut type of the sheet. |
Methods¶
Method | Description |
---|---|
GetClosedCornerDiameter | The diameter expression of the closed corner. |
GetEndValue | THE miter end value expression. |
GetStartValue | THE miter start value expression. |
SetClosedCornerDiameter | |
SetEndValue | |
SetStartValue |
Enumerations¶
MiterOptionsClosedCornerTypeOptions Enumeration | the closed corner type options. |
MiterOptionsPositionOptions Enumeration | the miter positions options. |
MiterOptionsTypeOptions Enumeration | the miter type options. |
Property Detail¶
ClosedCornerType¶
-
MiterOptions.
ClosedCornerType
¶ Returns or sets the closed corner option type.
-------------------------------------
Getter Method
Signature
ClosedCornerType()
Returns: Return type: NXOpen.Features.SheetMetal.MiterOptionsClosedCornerTypeOptions
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClosedCornerType(cutType)
Parameters: cutType ( NXOpen.Features.SheetMetal.MiterOptionsClosedCornerTypeOptions
) –New in version NX4.0.0.
License requirements: None.
ClosedCornerVAngle1¶
-
MiterOptions.
ClosedCornerVAngle1
¶ Returns the v cutout angle1 expression of the closed corner.
Applicable only when
NXOpen.Features.SheetMetal.MiterOptions.ClosedCornerTypeOptions
isFeatures.SheetMetal.MiterOptionsClosedCornerTypeOptions.VCutout
.-------------------------------------
Getter Method
Signature
ClosedCornerVAngle1()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
ClosedCornerVAngle2¶
-
MiterOptions.
ClosedCornerVAngle2
¶ Returns the v cutout angle2 expression of the closed corner.
Applicable only when
NXOpen.Features.SheetMetal.MiterOptions.ClosedCornerTypeOptions
isFeatures.SheetMetal.MiterOptionsClosedCornerTypeOptions.VCutout
.-------------------------------------
Getter Method
Signature
ClosedCornerVAngle2()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
EndType¶
-
MiterOptions.
EndType
¶ Returns or sets the miter end type.
-------------------------------------
Getter Method
Signature
EndType()
Returns: Return type: NXOpen.Features.SheetMetal.MiterOptionsTypeOptions
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndType(endType)
Parameters: endType ( NXOpen.Features.SheetMetal.MiterOptionsTypeOptions
) –New in version NX4.0.0.
License requirements: None.
MiterInteriorCornersIfNecessary¶
-
MiterOptions.
MiterInteriorCornersIfNecessary
¶ Returns or sets the miter_corners option.
If set to true, it miter bend edges that are larger than default bend radius.
-------------------------------------
Getter Method
Signature
MiterInteriorCornersIfNecessary()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MiterInteriorCornersIfNecessary(miterCorners)
Parameters: miterCorners (bool) – New in version NX5.0.0.
License requirements: None.
Position¶
-
MiterOptions.
Position
¶ Returns or sets the position of miter.
-------------------------------------
Getter Method
Signature
Position()
Returns: Return type: NXOpen.Features.SheetMetal.MiterOptionsPositionOptions
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Position(miterPosition)
Parameters: miterPosition ( NXOpen.Features.SheetMetal.MiterOptionsPositionOptions
) –New in version NX4.0.0.
License requirements: None.
StartType¶
-
MiterOptions.
StartType
¶ Returns or sets the miter start type.
-------------------------------------
Getter Method
Signature
StartType()
Returns: Return type: NXOpen.Features.SheetMetal.MiterOptionsTypeOptions
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartType(startType)
Parameters: startType ( NXOpen.Features.SheetMetal.MiterOptionsTypeOptions
) –New in version NX4.0.0.
License requirements: None.
UseNormalCutoutMethod¶
-
MiterOptions.
UseNormalCutoutMethod
¶ Returns or sets the cut type of the sheet.
If set to true, mitering is done using the normal cutout method and aims to reduce the small segements that result as part of miter computation, and is carried out on an unbent sheet. Normally, the cut runs through from one bend centre to another. The sheet is later bent to achieve the desired result.
-------------------------------------
Getter Method
Signature
UseNormalCutoutMethod()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseNormalCutoutMethod(cutType)
Parameters: cutType (bool) – New in version NX4.0.0.
License requirements: None.
Method Detail¶
GetClosedCornerDiameter¶
-
MiterOptions.
GetClosedCornerDiameter
¶ The diameter expression of the closed corner.
Applicable only when
NXOpen.Features.SheetMetal.MiterOptions.ClosedCornerTypeOptions
isFeatures.SheetMetal.MiterOptionsClosedCornerTypeOptions.CircularCutout
orFeatures.SheetMetal.MiterOptionsClosedCornerTypeOptions.UCutout
orFeatures.SheetMetal.MiterOptionsClosedCornerTypeOptions.VCutout
.Signature
GetClosedCornerDiameter()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
GetEndValue¶
-
MiterOptions.
GetEndValue
¶ THE miter end value expression.
Signature
GetEndValue()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
GetStartValue¶
-
MiterOptions.
GetStartValue
¶ THE miter start value expression.
Positive value adds material and negative v
Signature
GetStartValue()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
SetClosedCornerDiameter¶
-
MiterOptions.
SetClosedCornerDiameter
¶ Signature
SetClosedCornerDiameter(endValue)
Parameters: endValue (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: None.
SetEndValue¶
-
MiterOptions.
SetEndValue
¶ Signature
SetEndValue(endValue)
Parameters: endValue (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide
on theNXOpen.Expression
object returned fromFeatures.SheetMetal.MiterOptions.GetEndValue
instead.License requirements: None.
SetStartValue¶
-
MiterOptions.
SetStartValue
¶ Signature
SetStartValue(startValue)
Parameters: startValue (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide
on theNXOpen.Expression
object returned fromFeatures.SheetMetal.MiterOptions.GetStartValue
instead.License requirements: None.