DrawnCutoutBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
DrawnCutoutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Drawn Cutout feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateDrawnCutoutFeatureBuilder
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
CornerRadius | Returns the Radius to be applied for rounding the sharp section corners |
CutoutDepth | Returns the depth of the Drawn Cutout |
DepthType | Returns or sets the Direction in which the Drawn Cutout is punched. |
FilletSectionCorners | Returns or sets the Rounding Option for section Corners which contain Non Fillet Radii |
IncludeRounding | Returns or sets the Rounding type of the Sharp edges of bottom face and top face. |
MinimumToolClearance | Returns the minimum tool clearance expression. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RadiusOfDie | Returns the Radius value of the sharp edges of the bottom face |
Section | Returns or sets the Section used by the Drawn Cutout. |
SectionSide | Returns or sets the section side for the Drawn Cutout. |
SideAngle | Returns the Side Angle used by the Drawn Cutout. |
SidewallType | Returns or sets the side where the material must be added to the Drawn Cutout. |
Sketch | Returns or sets the Slave Sketch used by the Drawn Cutout, If one exists. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetCornerRadius | |
SetCutoutDepth | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRadiusOfDie | |
SetSideAngle | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify whether the builder data is valid for creating a Drawn Cutout or not. |
Enumerations¶
DrawnCutoutBuilderDepthTypeOptions Enumeration | This enum represents the depth direction for the drawn cutout. |
DrawnCutoutBuilderSectionSideOptions Enumeration | This enum represents the side of the section that the drawn cutout punches material. |
DrawnCutoutBuilderSidewallTypeOptions Enumeration | The side walls material option. |
Property Detail¶
CornerRadius¶
-
DrawnCutoutBuilder.
CornerRadius
¶ Returns the Radius to be applied for rounding the sharp section corners
-------------------------------------
Getter Method
Signature
CornerRadius()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
CutoutDepth¶
-
DrawnCutoutBuilder.
CutoutDepth
¶ Returns the depth of the Drawn Cutout
-------------------------------------
Getter Method
Signature
CutoutDepth()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
DepthType¶
-
DrawnCutoutBuilder.
DepthType
¶ Returns or sets the Direction in which the Drawn Cutout is punched.
This is used to specify the direction in which the punching should happen. If Punching must happen in the direction of the Section Normal (see
NXOpen.Features.SheetMetal.DrawnCutoutBuilder.Section
) then pass the value ofNXOpen.Features.SheetMetal.DrawnCutoutBuilderDepthTypeOptions.SectionNormalSide
If punching must happen in the opposite direction to that of Section Normal, set the value to beNXOpen.Features.SheetMetal.DrawnCutoutBuilderDepthTypeOptions.SectionReverseNormalSide
-------------------------------------
Getter Method
Signature
DepthType()
Returns: Return type: NXOpen.Features.SheetMetal.DrawnCutoutBuilderDepthTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
DepthType(depthType)
Parameters: depthType ( NXOpen.Features.SheetMetal.DrawnCutoutBuilderDepthTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
FilletSectionCorners¶
-
DrawnCutoutBuilder.
FilletSectionCorners
¶ Returns or sets the Rounding Option for section Corners which contain Non Fillet Radii
-------------------------------------
Getter Method
Signature
FilletSectionCorners()
Returns: Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
FilletSectionCorners(filletSectionCorners)
Parameters: filletSectionCorners (bool) – New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
IncludeRounding¶
-
DrawnCutoutBuilder.
IncludeRounding
¶ Returns or sets the Rounding type of the Sharp edges of bottom face and top face.
-------------------------------------
Getter Method
Signature
IncludeRounding()
Returns: Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
IncludeRounding(roundType)
Parameters: roundType (bool) – New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
MinimumToolClearance¶
-
DrawnCutoutBuilder.
MinimumToolClearance
¶ Returns the minimum tool clearance expression.
-------------------------------------
Getter Method
Signature
MinimumToolClearance()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
RadiusOfDie¶
-
DrawnCutoutBuilder.
RadiusOfDie
¶ Returns the Radius value of the sharp edges of the bottom face
-------------------------------------
Getter Method
Signature
RadiusOfDie()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Section¶
-
DrawnCutoutBuilder.
Section
¶ Returns or sets the Section used by the Drawn Cutout.
Section can be Open/Closed.
The section is protruded on the reference face at finite distance of extent and in the direction of extent side. The actual extent distance will be determined by the active dimension option i.e. Offset Dimension or Full Dimension. In case of Offset Dimension the actual extent distance will be offset dimension distance plus the thickness of sheet. In case of Full Dimension the actual extent distance will be the Full dimension distance. In case of open section, the end segments are extended to the nearest flat face edges. If the end segments are already crossing the flat face edges, those segments will be trimmed to the edges.
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Section(section)
Parameters: section ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SectionSide¶
-
DrawnCutoutBuilder.
SectionSide
¶ Returns or sets the section side for the Drawn Cutout.
This is used to specify which side of the section should remain stationary during the drawn cutout operation. drawn cutout’s section is a set of connected curves. The material exists on both sides of the section curves. section Side specifies - the material on which side of the curve must be punched.The other side shall be bent to the specified angle with respect to this fixed side. This is how you calculate Left/Right. Get the Section Normal (N)Get the Tangent of the section.(T) Result = CrossProduct(N, T). The resultant vector is called RIGHT. This vector shall be in the direction of one if the two sides of the material.If you want the material on the side of Result to be punched, then you have to pass the value of
NXOpen.Features.SheetMetal.DrawnCutoutBuilderSectionSideOptions.Right
If you want the other side to be punched, then you have to sendNXOpen.Features.SheetMetal.DrawnCutoutBuilderSectionSideOptions.Left
.-------------------------------------
Getter Method
Signature
SectionSide()
Returns: Return type: NXOpen.Features.SheetMetal.DrawnCutoutBuilderSectionSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
SectionSide(sectionSide)
Parameters: sectionSide ( NXOpen.Features.SheetMetal.DrawnCutoutBuilderSectionSideOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SideAngle¶
-
DrawnCutoutBuilder.
SideAngle
¶ Returns the Side Angle used by the Drawn Cutout.
In case of a tapered drawn cutout, the side angle is applied on the side faces of the above-protruded section. The affects of side angle will always increases the cavity volume of the drawn cutout.
-------------------------------------
Getter Method
Signature
SideAngle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SidewallType¶
-
DrawnCutoutBuilder.
SidewallType
¶ Returns or sets the side where the material must be added to the Drawn Cutout.
Done with Respect to the section
If
NXOpen.Features.SheetMetal.DrawnCutoutBuilderSidewallTypeOptions.Inside
is specified, the material of the drawn cutout sidewalls will be added to the interior of the section. IfNXOpen.Features.SheetMetal.DrawnCutoutBuilderSidewallTypeOptions.Outside
is specified,the material will be added from the lifted section such that the volume of the drawn cutout cavity is increased.-------------------------------------
Getter Method
Signature
SidewallType()
Returns: Return type: NXOpen.Features.SheetMetal.DrawnCutoutBuilderSidewallTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
SidewallType(sidewallType)
Parameters: sidewallType ( NXOpen.Features.SheetMetal.DrawnCutoutBuilderSidewallTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Sketch¶
-
DrawnCutoutBuilder.
Sketch
¶ Returns or sets the Slave Sketch used by the Drawn Cutout, If one exists.
If the Sketch is created internally as part of the Drawn Cutout command in the UI, then it shall be consumed by the Drawn Cutout and shall not show up as a seperate feature in the Part Navigator. If such a behaviour is deired, then specify the Sketch here.
-------------------------------------
Getter Method
Signature
Sketch()
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Sketch(sketch)
Parameters: sketch ( NXOpen.Features.SketchFeature
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
SetCornerRadius¶
-
DrawnCutoutBuilder.
SetCornerRadius
¶ Signature
SetCornerRadius(cornerRadius)
Parameters: cornerRadius (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.DrawnCutoutBuilder.CornerRadius
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetCutoutDepth¶
-
DrawnCutoutBuilder.
SetCutoutDepth
¶ Signature
SetCutoutDepth(depth)
Parameters: depth (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.DrawnCutoutBuilder.CutoutDepth
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetRadiusOfDie¶
-
DrawnCutoutBuilder.
SetRadiusOfDie
¶ Signature
SetRadiusOfDie(dieRadius)
Parameters: dieRadius (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.DrawnCutoutBuilder.RadiusOfDie
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
SetSideAngle¶
-
DrawnCutoutBuilder.
SetSideAngle
¶ Signature
SetSideAngle(sideAngle)
Parameters: sideAngle (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.DrawnCutoutBuilder.SideAngle
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”)
Validate¶
-
DrawnCutoutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
DrawnCutoutBuilder.
ValidateBuilderData
¶ Verify whether the builder data is valid for creating a Drawn Cutout or not.
If the Builder data is valid, returned value shall be 0
Signature
ValidateBuilderData()
Returns: Data Validity Flag. Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)