AeroSheetmetalManager Class¶
-
class
NXOpen.Features.SheetMetal.
AeroSheetmetalManager
¶ Bases:
object
Provides methods for manipulating the Knowledge Fusion rules in a part
To obtain an instance of this class, refer to
NXOpen.Features.FeatureCollection
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateAeroLighteningCutoutBuilder | Creates a NXOpen.Features.SheetMetal.AeroLighteningCutoutBuilder @return AeroLighteningCutoutBuilder object |
CreateFlangeBuilder | Create flange builder @return AeroFlangeBuilder object |
CreateFlatPatternBuilder | Creates a NXOpen.Features.SheetMetal.FlatPatternBuilder @return FlatPatternBuilder object |
CreateFlatSolidBuilder | Create flat solid builder @return FlatSolidBuilder object |
CreateJoggleBuilder | Create joggle builder @return AeroJoggleBuilder object |
CreateReformBuilder | Create reform builder @return AeroReformBuilder object |
CreateUnformBuilder | Create unform builder @return AeroUnformBuilder object |
Method Detail¶
CreateAeroLighteningCutoutBuilder¶
-
AeroSheetmetalManager.
CreateAeroLighteningCutoutBuilder
¶ Creates a
NXOpen.Features.SheetMetal.AeroLighteningCutoutBuilder
Signature
CreateAeroLighteningCutoutBuilder(aeroLighteningCutout)
Parameters: aeroLighteningCutout ( NXOpen.Features.Feature
) –NXOpen.Features.Feature
to be editedReturns: AeroLighteningCutoutBuilder object Return type: NXOpen.Features.SheetMetal.AeroLighteningCutoutBuilder
New in version NX5.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
CreateFlangeBuilder¶
-
AeroSheetmetalManager.
CreateFlangeBuilder
¶ Create flange builder
Signature
CreateFlangeBuilder(aerosmFlange)
Parameters: aerosmFlange ( NXOpen.Features.Feature
) –NXOpen.Features.SheetMetal.AeroFlangeBuilder
to be edited, if None then create a new oneReturns: AeroFlangeBuilder object Return type: NXOpen.Features.SheetMetal.AeroFlangeBuilder
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
CreateFlatPatternBuilder¶
-
AeroSheetmetalManager.
CreateFlatPatternBuilder
¶ Creates a
NXOpen.Features.SheetMetal.FlatPatternBuilder
Signature
CreateFlatPatternBuilder(aerosmUnform)
Parameters: aerosmUnform ( NXOpen.Features.Feature
) –NXOpen.Features.Feature
to be edited, if None then create a new oneReturns: FlatPatternBuilder object Return type: NXOpen.Features.SheetMetal.FlatPatternBuilder
New in version NX6.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
CreateFlatSolidBuilder¶
-
AeroSheetmetalManager.
CreateFlatSolidBuilder
¶ Create flat solid builder
Signature
CreateFlatSolidBuilder(aerosmUnform)
Parameters: aerosmUnform ( NXOpen.Features.Feature
) –NXOpen.Features.SheetMetal.FlatSolidBuilder
to be edited, if None then create a new oneReturns: FlatSolidBuilder object Return type: NXOpen.Features.SheetMetal.FlatSolidBuilder
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
CreateJoggleBuilder¶
-
AeroSheetmetalManager.
CreateJoggleBuilder
¶ Create joggle builder
Signature
CreateJoggleBuilder(aerosmJoggle)
Parameters: aerosmJoggle ( NXOpen.Features.Feature
) –NXOpen.Features.SheetMetal.AeroJoggleBuilder
to be edited, if None then create a new oneReturns: AeroJoggleBuilder object Return type: NXOpen.Features.SheetMetal.AeroJoggleBuilder
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
CreateReformBuilder¶
-
AeroSheetmetalManager.
CreateReformBuilder
¶ Create reform builder
Signature
CreateReformBuilder(aerosmReform)
Parameters: aerosmReform ( NXOpen.Features.Feature
) –NXOpen.Features.SheetMetal.AeroReformBuilder
to be edited, if None then create a new oneReturns: AeroReformBuilder object Return type: NXOpen.Features.SheetMetal.AeroReformBuilder
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
CreateUnformBuilder¶
-
AeroSheetmetalManager.
CreateUnformBuilder
¶ Create unform builder
Signature
CreateUnformBuilder(aerosmUnform)
Parameters: aerosmUnform ( NXOpen.Features.Feature
) –NXOpen.Features.SheetMetal.AeroUnformBuilder
to be edited, if None then create a new oneReturns: AeroUnformBuilder object Return type: NXOpen.Features.SheetMetal.AeroUnformBuilder
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)