AeroFlangeBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
AeroFlangeBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Aerospace Sheet Metal Flange Builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.AeroSheetmetalManager.CreateFlangeBuilder
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle expression. |
BaseEdges | Returns or sets the base edge section object for the flange. |
BendOptions | Returns the base edge section object for the flange. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RefFaces | Returns or sets the ref face smart collector object |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetContourFlag | Get the flag that turns on/off the visibility of Contour Curve @return false = Hide contour curve, true = Show contour curve |
GetDimensionType | Get the length dimension type of the flange @return inside/outside |
GetEndCompensation | Get end compensation. |
GetEndPlane | Get the end plane @return smart plane entity |
GetFeature | Returns the feature currently being edited by this builder. |
GetFlipDirection | Get flip direction. |
GetLength | Get the type of length and the length expression. |
GetMaterialType | Get the material type of the flange @return material inside/material outside/bend outside |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetAngle | Set the angle expression. |
SetApplicationContext | Set the application context. |
SetContourFlag | Set the flag that turns on/off the visibility of Contour Curve |
SetDimensionType | Set the length dimension type of the flange |
SetEndCompensation | Set end compensation. |
SetEndPlane | Set the end plane |
SetFlipDirection | Set flip direction. |
SetLength | Set the type of length and the length expression. |
SetMaterialType | Set the material type of the flange |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AeroFlangeBuilderCompType Enumeration | This method defines the types of Flange Compensation |
AeroFlangeBuilderDimType Enumeration | This enum defines the flange length dimension types |
AeroFlangeBuilderDirType Enumeration | This enum defines the type of direction vector |
AeroFlangeBuilderEndType Enumeration | This enum defines the ends of a bend edge |
AeroFlangeBuilderLengthType Enumeration | This enum defines the length type options. |
AeroFlangeBuilderMatType Enumeration | This enum defines the material types |
Property Detail¶
Angle¶
-
AeroFlangeBuilder.
Angle
¶ Returns the angle expression.
-------------------------------------
Getter Method
Signature
Angle()
Returns: angle expression Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
BaseEdges¶
-
AeroFlangeBuilder.
BaseEdges
¶ Returns or sets the base edge section object for the flange.
-------------------------------------
Getter Method
Signature
BaseEdges()
Returns: Base Edges Return type: NXOpen.ScCollector
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
-------------------------------------
Setter Method
Signature
BaseEdges(baseEdges)
Parameters: baseEdges ( NXOpen.ScCollector
) – Base EdgesNew in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
BendOptions¶
-
AeroFlangeBuilder.
BendOptions
¶ Returns the base edge section object for the flange.
-------------------------------------
Getter Method
Signature
BendOptions()
Returns: Bend Options Return type: NXOpen.Features.SheetMetal.BendOptions
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
RefFaces¶
-
AeroFlangeBuilder.
RefFaces
¶ Returns or sets the ref face smart collector object
-------------------------------------
Getter Method
Signature
RefFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
-------------------------------------
Setter Method
Signature
RefFaces(faceCollector)
Parameters: faceCollector ( NXOpen.ScCollector
) –New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Method Detail¶
GetContourFlag¶
-
AeroFlangeBuilder.
GetContourFlag
¶ Get the flag that turns on/off the visibility of Contour Curve
Signature
GetContourFlag()
Returns: false = Hide contour curve, true = Show contour curve Return type: bool New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetDimensionType¶
-
AeroFlangeBuilder.
GetDimensionType
¶ Get the length dimension type of the flange
Signature
GetDimensionType()
Returns: inside/outside Return type: NXOpen.Features.SheetMetal.AeroFlangeBuilderDimType
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetEndCompensation¶
-
AeroFlangeBuilder.
GetEndCompensation
¶ Get end compensation.
Signature
GetEndCompensation(endType)
Parameters: endType ( NXOpen.Features.SheetMetal.AeroFlangeBuilderEndType
) – end1/end2Returns: a tuple Return type: A tuple consisting of (valueExpression, compType). valueExpression is a NXOpen.Expression
. compensation expression compType is aNXOpen.Features.SheetMetal.AeroFlangeBuilderCompType
. Automatic/Angle/Distance/NoneNew in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetEndPlane¶
-
AeroFlangeBuilder.
GetEndPlane
¶ Get the end plane
Signature
GetEndPlane(endType)
Parameters: endType ( NXOpen.Features.SheetMetal.AeroFlangeBuilderEndType
) – end1/end2Returns: smart plane entity Return type: NXOpen.Plane
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetFlipDirection¶
-
AeroFlangeBuilder.
GetFlipDirection
¶ Get flip direction.
Signature
GetFlipDirection(type)
Parameters: type ( NXOpen.Features.SheetMetal.AeroFlangeBuilderDirType
) – direction type bend/discardReturns: flip_flag =<ja_gt> false = do not flip, true = flip Return type: bool New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetLength¶
-
AeroFlangeBuilder.
GetLength
¶ Get the type of length and the length expression.
Signature
GetLength()
Returns: a tuple Return type: A tuple consisting of (lengthExpression, type). lengthExpression is a NXOpen.Expression
. length expression type is aNXOpen.Features.SheetMetal.AeroFlangeBuilderLengthType
. length type Value/InferNew in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
GetMaterialType¶
-
AeroFlangeBuilder.
GetMaterialType
¶ Get the material type of the flange
Signature
GetMaterialType()
Returns: material inside/material outside/bend outside Return type: NXOpen.Features.SheetMetal.AeroFlangeBuilderMatType
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetAngle¶
-
AeroFlangeBuilder.
SetAngle
¶ Set the angle expression.
This method should be called only when there is no ref_face selection.
Signature
SetAngle(angleExpression)
Parameters: angleExpression (str) – value of angle expression NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetContourFlag¶
-
AeroFlangeBuilder.
SetContourFlag
¶ Set the flag that turns on/off the visibility of Contour Curve
Signature
SetContourFlag(showContour)
Parameters: showContour (bool) – false = Hide contour curve, true = Show contour curve New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetDimensionType¶
-
AeroFlangeBuilder.
SetDimensionType
¶ Set the length dimension type of the flange
Signature
SetDimensionType(dimType)
Parameters: dimType ( NXOpen.Features.SheetMetal.AeroFlangeBuilderDimType
) – inside/outsideNew in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
SetEndCompensation¶
-
AeroFlangeBuilder.
SetEndCompensation
¶ Set end compensation.
This method sets the flange compensation for one end of a non-periodic Base Edge section. The end_type input parameter denotes if the end is the start of section(end1) or the end of section(end2). If the compensation type( comp_type) is either Angle or Distance, an expression for the value of compensation must be provided. This expression input can be NULL for Automatic and None type of compensations.
Signature
SetEndCompensation(endType, compType, valueExpression)
Parameters: - endType (
NXOpen.Features.SheetMetal.AeroFlangeBuilderEndType
) – end1/end2 - compType (
NXOpen.Features.SheetMetal.AeroFlangeBuilderCompType
) – Automatic/Angle/Distance/None - valueExpression (str) – value of compensation expression NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
- endType (
SetEndPlane¶
-
AeroFlangeBuilder.
SetEndPlane
¶ Set the end plane
Signature
SetEndPlane(endType, endPlane)
Parameters: - endType (
NXOpen.Features.SheetMetal.AeroFlangeBuilderEndType
) – end1/end2 - endPlane (
NXOpen.Plane
) – smart plane entity
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
- endType (
SetFlipDirection¶
-
AeroFlangeBuilder.
SetFlipDirection
¶ Set flip direction.
This method is called if either the bend direction or the material direction needs to be flipped.
Signature
SetFlipDirection(type, flipFlag)
Parameters: - type (
NXOpen.Features.SheetMetal.AeroFlangeBuilderDirType
) – direction type bend/discard - flipFlag (bool) – flip_flag =<ja_gt> false = do not flip, true = flip
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
- type (
SetLength¶
-
AeroFlangeBuilder.
SetLength
¶ Set the type of length and the length expression.
If there are no ref_face’s then the only length type possible is “Value”. If there are selected ref_face’s and the length type is “Infer”, then the length expression should be NULL.
Signature
SetLength(type, valueExpression)
Parameters: - type (
NXOpen.Features.SheetMetal.AeroFlangeBuilderLengthType
) – length type input Value/Infer - valueExpression (str) – value of length expression NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
- type (
SetMaterialType¶
-
AeroFlangeBuilder.
SetMaterialType
¶ Set the material type of the flange
Signature
SetMaterialType(matType)
Parameters: matType ( NXOpen.Features.SheetMetal.AeroFlangeBuilderMatType
) – material inside/material outside/bend outsideNew in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”) OR adv_sheet_metal_dsgn (“ADVANCED SHEET METAL DESIGN”)
Validate¶
-
AeroFlangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.