RebendBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
RebendBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
The Rebend feature class.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateRebendFeatureBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FaceCollector | Returns or sets the unbent faces to rebend |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReferenceEntity | Returns or sets the non-thickness planar face or linear edge to remain fixed while part is rebent |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify whether the builder data is valid for creating Rebend or not. |
Property Detail¶
FaceCollector¶
-
RebendBuilder.
FaceCollector
¶ Returns or sets the unbent faces to rebend
-------------------------------------
Getter Method
Signature
FaceCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
FaceCollector(faceCollector)
Parameters: faceCollector ( NXOpen.ScCollector
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ReferenceEntity¶
-
RebendBuilder.
ReferenceEntity
¶ Returns or sets the non-thickness planar face or linear edge to remain fixed while part is rebent
-------------------------------------
Getter Method
Signature
ReferenceEntity()
Returns: Return type: NXOpen.NXObject
New in version NX7.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
ReferenceEntity(referenceEntity)
Parameters: referenceEntity ( NXOpen.NXObject
) –New in version NX7.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
Validate¶
-
RebendBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
RebendBuilder.
ValidateBuilderData
¶ Verify whether the builder data is valid for creating Rebend or not.
If the Builder data is valid, returned value shall be 0
Signature
ValidateBuilderData()
Returns: Return type: int New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)