FlexibleCableSegment Class¶
-
class
NXOpen.Features.SheetMetal.
FlexibleCableSegment
¶ Bases:
NXOpen.NXObject
Represents a Flexible Cable Segment class.
No creator as of now
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BendAngle | Returns the bend angle. |
BendAngleDirection | Returns or sets the bend angle direction. |
BendRadius | Returns the bend radius. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Length | Returns the length. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PathAdjustmentAngle | Returns the path adjustment angle. |
PathAdjustmentAngleDirection | Returns or sets the path adjustment angle direction. |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSegmentType | Returns the type of cable segment. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
BendAngle¶
-
FlexibleCableSegment.
BendAngle
¶ Returns the bend angle.
-------------------------------------
Getter Method
Signature
BendAngle()
Returns: Bend Angle. Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
BendAngleDirection¶
-
FlexibleCableSegment.
BendAngleDirection
¶ Returns or sets the bend angle direction.
-------------------------------------
Getter Method
Signature
BendAngleDirection()
Returns: Bend angle direction option. Return type: NXOpen.Features.SheetMetal.FlexibleCableBuilderBendAngleDirectionOptions
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
BendAngleDirection(bendAngleDirectionOption)
Parameters: bendAngleDirectionOption ( NXOpen.Features.SheetMetal.FlexibleCableBuilderBendAngleDirectionOptions
) – Bend angle direction option.New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
BendRadius¶
-
FlexibleCableSegment.
BendRadius
¶ Returns the bend radius.
-------------------------------------
Getter Method
Signature
BendRadius()
Returns: Bend Radius. Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
IsOccurrence¶
-
FlexibleCableSegment.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FlexibleCableSegment.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Length¶
-
FlexibleCableSegment.
Length
¶ Returns the length.
-------------------------------------
Getter Method
Signature
Length()
Returns: Length. Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
Name¶
-
FlexibleCableSegment.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FlexibleCableSegment.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FlexibleCableSegment.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PathAdjustmentAngle¶
-
FlexibleCableSegment.
PathAdjustmentAngle
¶ Returns the path adjustment angle.
-------------------------------------
Getter Method
Signature
PathAdjustmentAngle()
Returns: Path Adjustment Angle. Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
PathAdjustmentAngleDirection¶
-
FlexibleCableSegment.
PathAdjustmentAngleDirection
¶ Returns or sets the path adjustment angle direction.
-------------------------------------
Getter Method
Signature
PathAdjustmentAngleDirection()
Returns: Path adjustment angle direction option. Return type: NXOpen.Features.SheetMetal.FlexibleCableBuilderPathAdjustmentAngleDirectionOptions
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
PathAdjustmentAngleDirection(pathAdjustmentAngleDirectionOption)
Parameters: pathAdjustmentAngleDirectionOption ( NXOpen.Features.SheetMetal.FlexibleCableBuilderPathAdjustmentAngleDirectionOptions
) – Path adjustment angle direction option.New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
Prototype¶
-
FlexibleCableSegment.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
FlexibleCableSegment.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetSegmentType¶
-
FlexibleCableSegment.
GetSegmentType
¶ Returns the type of cable segment.
It could be of
NXOpen.Features.SheetMetal.FlexibleCableBuilderSegmentTypeOptions.Planar
, orNXOpen.Features.SheetMetal.FlexibleCableBuilderSegmentTypeOptions.Bend
Signature
GetSegmentType()
Returns: Cable segment type. Return type: NXOpen.Features.SheetMetal.FlexibleCableBuilderSegmentTypeOptions
New in version NX7.5.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”)
Print¶
-
FlexibleCableSegment.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FlexibleCableSegment.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.