ConvertToSheetmetalBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
ConvertToSheetmetalBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
This is the feature builder for the convert to sheetmetal feature.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateConvertToSheetmetalFeatureBuilder
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AdditionalFacesToConvert | Returns the additional faces to convert |
BaseFace | Returns or sets the base face from which the thickness of the part is determined. |
BendReliefDepth | Returns the bend relief depth. |
BendReliefType | Returns or sets the bend relief type. |
BendReliefWidth | Returns the bend relief width. |
MaintainZeroBendRadius | Returns or sets the option for Maintain zero bend radius. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RipSection | Returns or sets the section containing curves that need to be ripped while converting to sheetmetal. |
Sketch | Returns or sets the internal sketch (used to specify rip curves), if it exists. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetRipEdges | Gets the array of edges selected for ripping while converting to sheetmetal. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetBendReliefDepth | |
SetBendReliefWidth | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRipEdges | Sets the array of edges that need to be ripped while converting to sheetmetal. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify that the builder data is valid for feature creation. |
Enumerations¶
ConvertToSheetmetalBuilderBendReliefTypeOptions Enumeration | This enum represents the bend relief type. |
Property Detail¶
AdditionalFacesToConvert¶
-
ConvertToSheetmetalBuilder.
AdditionalFacesToConvert
¶ Returns the additional faces to convert
-------------------------------------
Getter Method
Signature
AdditionalFacesToConvert()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BaseFace¶
-
ConvertToSheetmetalBuilder.
BaseFace
¶ Returns or sets the base face from which the thickness of the part is determined.
-------------------------------------
Getter Method
Signature
BaseFace()
Returns: Return type: NXOpen.Face
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
BaseFace(baseFace)
Parameters: baseFace ( NXOpen.Face
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
BendReliefDepth¶
-
ConvertToSheetmetalBuilder.
BendReliefDepth
¶ Returns the bend relief depth.
-------------------------------------
Getter Method
Signature
BendReliefDepth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
BendReliefType¶
-
ConvertToSheetmetalBuilder.
BendReliefType
¶ Returns or sets the bend relief type.
-------------------------------------
Getter Method
Signature
BendReliefType()
Returns: Return type: NXOpen.Features.SheetMetal.ConvertToSheetmetalBuilderBendReliefTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
BendReliefType(bendReliefType)
Parameters: bendReliefType ( NXOpen.Features.SheetMetal.ConvertToSheetmetalBuilderBendReliefTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
BendReliefWidth¶
-
ConvertToSheetmetalBuilder.
BendReliefWidth
¶ Returns the bend relief width.
-------------------------------------
Getter Method
Signature
BendReliefWidth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
MaintainZeroBendRadius¶
-
ConvertToSheetmetalBuilder.
MaintainZeroBendRadius
¶ Returns or sets the option for Maintain zero bend radius.
If the option is set to true, a tiny 0.02 mm radius bend will be created on inside sharp edge (for the features created in NX8 or later releases); else the radius value from NXSM Preferences will be used.
-------------------------------------
Getter Method
Signature
MaintainZeroBendRadius()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
MaintainZeroBendRadius(maintainZeroBendRadius)
Parameters: maintainZeroBendRadius (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
RipSection¶
-
ConvertToSheetmetalBuilder.
RipSection
¶ Returns or sets the section containing curves that need to be ripped while converting to sheetmetal.
-------------------------------------
Getter Method
Signature
RipSection()
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
RipSection(section)
Parameters: section ( NXOpen.Section
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Sketch¶
-
ConvertToSheetmetalBuilder.
Sketch
¶ Returns or sets the internal sketch (used to specify rip curves), if it exists.
-------------------------------------
Getter Method
Signature
Sketch()
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
Sketch(sketch)
Parameters: sketch ( NXOpen.Features.SketchFeature
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
GetRipEdges¶
-
ConvertToSheetmetalBuilder.
GetRipEdges
¶ Gets the array of edges selected for ripping while converting to sheetmetal.
Signature
GetRipEdges()
Returns: Return type: list of NXOpen.Edge
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SetBendReliefDepth¶
-
ConvertToSheetmetalBuilder.
SetBendReliefDepth
¶ Signature
SetBendReliefDepth(bendReliefDepth)
Parameters: bendReliefDepth (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
Expression.RightHandSide
on theExpression
object returned fromFeatures.SheetMetal.ConvertToSheetmetalBuilder.BendReliefDepth
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SetBendReliefWidth¶
-
ConvertToSheetmetalBuilder.
SetBendReliefWidth
¶ Signature
SetBendReliefWidth(bendReliefWidth)
Parameters: bendReliefWidth (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
Expression.RightHandSide
on theExpression
object returned fromFeatures.SheetMetal.ConvertToSheetmetalBuilder.BendReliefWidth
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SetRipEdges¶
-
ConvertToSheetmetalBuilder.
SetRipEdges
¶ Sets the array of edges that need to be ripped while converting to sheetmetal.
Signature
SetRipEdges(ripEdges)
Parameters: ripEdges (list of NXOpen.Edge
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Validate¶
-
ConvertToSheetmetalBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
ConvertToSheetmetalBuilder.
ValidateBuilderData
¶ Verify that the builder data is valid for feature creation.
If the builder data is valid, it returns a value of 0.
Signature
ValidateBuilderData()
Returns: data validity flag (0 - valid, 1 - invalid) Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)