ActiveDocument | Returns the currently active document. |
ActiveDocumentType | Returns the type of the currently active document. |
ActiveEnvironment | Returns the environment that belongs to the current active window of the document. |
ActiveObject | Returns an Object from the active document. The type of object returned is specified by Type. |
ActivePrinter | Returns the name of the active printer. |
ActiveSelectSet | Returns the SelectSet object for the currently active window. |
ActiveStatusBarPart | Sets and returns the current active status bar part. |
ActiveWindow | Returns the active Window object. |
AddIns | Returns the AddIns object for the referenced Application object. |
Application | Returns the active application object. |
ApplicationEvents | Returns the ApplicationEvents object for the referenced Application object. |
ApplicationV8AfterDocumentOpenEvent | Returns the ApplicationV8DocumentOpenEvent object for the referenced Application object. |
ApplicationWindowEvents | Returns the ApplicationWindowEvents object for the referenced Application object. |
ApprenticeMode | |
BeforeFileSaveAsEvents | Returns the BeforeFileSaveAsEvents object for the referenced Application object. |
Caption | Sets and returns the caption of the referenced object. |
Customization | An object that is used to customize the user interface. |
DefaultFilePath | Sets and returns the default path used when files are opened. |
DelayCompute | Specifies whether or not to suspend the computing process. |
DisplayAlerts | Enables or disables the display of alerts and messages. |
DisplayFullScreen | Specifies whether or not the referenced Application object is maximized. |
DisplayRecentFiles | Specifies whether or not the used file list is appended to the File menu of the referenced Application object. |
DisplayRecentFilesCount | Sets and returns the number of files that are displayed in the most recently used (MRU) list. |
Documents | Returns the collection of documents that are owned by the referenced Application object. |
EdgeBarVisible | Specifies whether or not the Edge Bar is visible for the referenced Application object. |
EnableStereo | Specifies whether or not the referenced Application object will support the creation of stereoscopic displays. |
Environments | Returns a collection of Environment objects that are owned by the referenced Application object. |
FeatureLibraryEvents | Returns the FeatureLibraryEvents object for the referenced Application object. |
FileUIEvents | Returns the FileUIEvents object for the referenced Application object. |
Height | Returns the height of the referenced object. |
hWnd | Returns the window handle for the referenced object. |
Insight | This read-only property returns the Insight object. |
Interactive | Specifies whether or not the referenced Application object can be used interactively. |
IsIdling | |
Left | Specifies the distance (in twips) between the internal left edge of an object and the left edge of its container. |
MailSession | Returns the MAPI mail session number. |
Name | Returns the name of the referenced object. |
NewFileUIEvents | Returns the NewFileUIEvents object for the referenced Application object. |
Parent | Returns the parent object for the referenced object. |
ProcessID | Returns the processID of the application. |
ScreenUpdating | Determines if the screen updating is enabled or disabled. |
SEECEvents | |
SESPEvents | |
ShortcutMenuEvents | Returns the ShortcutMenuEvents object for the referenced Application object. |
ShowStartupScreen | |
SolidEdgeInsightXT | |
SolidEdgeTCE | |
StatusBar | Sets and returns the caption text that is displayed in the referenced Application object. |
StatusBarDelayUpdate | Specifies whether to immediately update the status bar or to defer the update to the idle loop. |
StatusBarHeight | Returns the height of the status bar. |
StatusBarPartCount | Sets and returns the number of parts or sections into which the status bar is divided. |
StatusBarPartWidth | Returns the width of the current active part of the status bar. |
StatusBarVisible | Specifies whether or not the status bar is visible. |
Top | Sets and returns the distance from the top of the screen to the top of the referenced object or control. |
UsableHeight | Returns the height of the usable vertical space in the application window. |
UsableWidth | Returns the width of the usable horizontal space in the application window area. |
UserName | Returns the name of the current user. |
Value | Returns the name of the application, the value of a dimension, the value of a custom property, or the value of a variable. |
Version | Returns the version number of the referenced Application object. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
Width | Returns the width of the referenced object. |
Windows | Returns a collection of Window objects. |
WindowState | Returns or sets the state of the referenced window. |