Solid Edge Framework Type Library
ApplicationEvents Property
Description
Returns the ApplicationEvents object for the referenced Application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property ApplicationEvents As ApplicationEvents
Example
Imports SolidEdgeFramework
Imports System.Runtime.InteropServices

Public Class Form1
    Private objApplication As SolidEdgeFramework.Application
    Private WithEvents objAppEvents As SolidEdgeFramework.ISEApplicationEvents_Event

    Private Sub Form1_Load(ByVal sender As System.Object, ByVal e As System.EventArgs) Handles MyBase.Load
        Try
            OleMessageFilter.Register()

            ' Connect to a running instance of Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            ' Get a reference to the application events
            objAppEvents = objApplication.ApplicationEvents
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        End Try
    End Sub

    Private Sub Form1_FormClosing(ByVal sender As System.Object, ByVal e As System.Windows.Forms.FormClosingEventArgs) Handles MyBase.FormClosing
        If Not (objAppEvents Is Nothing) Then
            Marshal.ReleaseComObject(objAppEvents)
            objAppEvents = Nothing
        End If
        If Not (objApplication Is Nothing) Then
            Marshal.ReleaseComObject(objApplication)
            objApplication = Nothing
        End If
        OleMessageFilter.Revoke()
    End Sub
End Class
See Also

Application Object  | Application Members