Solid Edge Framework Type Library
GetDraftPrintUtility Method
Description
An object that is used to print Draft files.
Syntax
Visual Basic
Public Function GetDraftPrintUtility() As Object
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftPrintUtility As SolidEdgeDraft.DraftPrintUtility = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objDraftPrintUtility = objApplication.GetDraftPrintUtility()

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Application Object  | Application Members  | Solid Edge ST3 - What's New