Solid Edge Framework Type Library
DisplayRecentFilesCount Property
Description
Sets and returns the number of files that are displayed in the most recently used (MRU) list.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayRecentFilesCount As Long
Remarks
A maximum of 16 files can be maintained in the MRU list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim lngDispFil As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Set the RecentFilesCount value
    objApp.DisplayRecentFilesCount = 10
    ' Get the DisplayRecentFilesCount property
    lngDispFil = objApp.DisplayRecentFilesCount
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
End Sub
See Also

Application Object  | Application Members