Solid Edge Framework Type Library
StatusBar Property
Description
Sets and returns the caption text that is displayed in the referenced Application object.
Property type
Read-write property
Syntax
Visual Basic
Public Property StatusBar As String
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim strStatBar As String
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Get the StatusBar property
    strStatBar = objApp.StatusBar
    ' Set the StatusBar caption text
    objApp.StatusBar = "PartDocument"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
End Sub
See Also

Application Object  | Application Members