Solid Edge Framework Type Library
StatusBarDelayUpdate Property
Description
Specifies whether to immediately update the status bar or to defer the update to the idle loop.
Property type
Read-write property
Syntax
Visual Basic
Public Property StatusBarDelayUpdate As Boolean
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim bDelUpdt As Boolean
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Get the StatusBarDelayUpdate property
    bDelUpdt = objApp.StatusBarDelayUpdate
    ' Reset the property
    objApp.StatusBarDelayUpdate = Not bDelUpdt
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
End Sub
See Also

Application Object  | Application Members