Solid Edge Framework Type Library
SetOLERequestPendingTimeout Method
Specifies the number of milliseconds. The default value is 8000 milliseconds (8 seconds).
Description
Determines in milliseconds the amount of time after an automation or OLE request is made before a busy message is displayed. The default value is 8000 milliseconds (8 seconds)
Syntax
Visual Basic
Public Sub SetOLERequestPendingTimeout( _
   Optional ByVal SetOLERequestPendingTimeout As Variant _
) 
Parameters
SetOLERequestPendingTimeout
Specifies the number of milliseconds. The default value is 8000 milliseconds (8 seconds).
See Also

Application Object  | Application Members