Solid Edge Framework Type Library
DisplayRecentFiles Property
Description
Specifies whether or not the used file list is appended to the File menu of the referenced Application object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayRecentFiles As Boolean
Remarks
If True, the list is appended to the File menu.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim bDispFil As Boolean
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Get the Intial Boolean value of DisplayRecentFiles property
    bDispFil = objApp.DisplayRecentFiles
    'Turn off the display of RecentFiles list
    objApp.DisplayRecentFiles = Not bDispFil
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
End Sub
See Also

Application Object  | Application Members