Solid Edge Framework Type Library
UsableWidth Property
Description
Returns the width of the usable horizontal space in the application window area.
Property type
Read-only property
Syntax
Visual Basic
Public Property UsableWidth As Integer
Remarks
The width is returned in points (1/72 inch). Adding section tabs or a vertical scroll bar reduces the usable width.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim iUWidth As Integer
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Get the UsableWidth of the Application
    iUWidth = objApp.UsableWidth
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
End Sub
See Also

Application Object  | Application Members