Solid Edge Framework Type Library
SetOLEServerBusyTimeout Method
Specifies the number of milliseconds. The default value is 10000 milliseconds (10 seconds).
Description
Determines in milliseconds how long Solid Edge will go on retrying your automation or OLE requests before displaying the Component Busy dialog. The default value is 10000 milliseconds (10 seconds).
Syntax
Visual Basic
Public Sub SetOLEServerBusyTimeout( _
   Optional ByVal SetOLEServerBusyTimeout As Variant _
) 
Parameters
SetOLEServerBusyTimeout
Specifies the number of milliseconds. The default value is 10000 milliseconds (10 seconds).
See Also

Application Object  | Application Members