Solid Edge Framework Type Library
Top Property
Description
Sets and returns the distance from the top of the screen to the top of the referenced object or control.
Property type
Read-write property
Syntax
Visual Basic
Public Property Top As Integer
Remarks
Sets and returns the distance from the top edge of the physical screen to the top edge of the main application window, in points (1/72 inch).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim iTop As Integer
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Get the Top property
    iTop = objApp.Top
    ' Set the Top property
    objApp.Top = 0
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
End Sub
See Also

Application Object  | Application Members