FilletBuilder Class¶
-
class
NXOpen.Weld.
FilletBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Weld.Fillet
builder.To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateFilletBuilder()
Default values.
Property Value AddCosmeticEnd 0 AllowBroken 0 AssignWeldPMI 0 Associative 1 ContourHeight.Value 1.875 (millimeters part), .073818 (inches part) ContourType None EnumMethod NumberLength ExtendEdges Manual ExtensionDistance.Value 0.0254 (millimeters part), 0.001 (inches part) ExtensionMethod Automatic FaceFillGapDistance 0.0 (millimeters part), 0.0 (inches part) FieldWeld 0 FillFaceHoles None FilletType T FirstLeg.Value 6.25 (millimeters part), .246062 (inches part) NumberOfWelds.Value 3 SecondLeg.Value 6.25 (millimeters part), .246062 (inches part) SegmentLength.Value 3 (millimeters part), .118110 (inches part) Spacing.Value 3 (millimeters part), .118110 (inches part) ThroatThickToggle 0 ToggleCreateSkipWelds 0 ToggleRecreateDeletedWelds 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AddCosmeticEnd | Returns or sets the value identify if a cosmtic end should be added to each end of the fillet. |
AllowBroken | Returns or sets the toggle to allow broken link. |
AssignWeldPMI | Returns or sets the toggle to assign weld pmi. |
Associative | Returns or sets the value identify if WAVE links should remain unbroken. |
ConstructionMethod | Returns or sets the value for determining the construction method. |
ContourHeight | Returns the linear dimension contour height. |
ContourType | Returns or sets the contour. |
DirectToggle | Returns or sets the toggle to change direction. |
DirectionVector1 | Returns or sets the face normal direction. |
DirectionVector2 | Returns or sets the face normal direction for the second face. |
DistTolerance | Returns or sets the distance tolerance. |
EdgeSet1 | Returns the edge set1. |
EdgeSet2 | Returns the edge set2. |
EndDist | Returns the on path dimension end distance. |
EndVector | Returns or sets the end direction reversed or not. |
EnumMethod | Returns or sets the enum method for skip welds. |
ExtendEdges | Returns or sets the value for how to populate the edge sets. |
ExtensionDistance | Returns the linear dimension extension distance. |
ExtensionMethod | Returns or sets the extension method. |
FaceFillGapDistance | Returns or sets the distance the fillet will span when there are gaps in the sheet definition. |
FaceSet1 | Returns the face set1. |
FaceSet2 | Returns the face set2. |
FieldWeld | Returns or sets the field weld. |
FillFaceHoles | Returns or sets the value to identify if the face set should be filled during construction. |
FilletType | Returns or sets the fillet type. |
FirstLeg | Returns the linear dimension first leg. |
NumberOfWelds | Returns the expression number indicates number of welds in skip welds. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Pmi | Returns or sets the pmi symbol. |
SecondLeg | Returns the linear dimension second leg. |
SeedFace1 | Returns or sets the first seed face. |
SeedFace2 | Returns or sets the second seed face. |
SeedPoint1 | Returns or sets the point on the first face. |
SeedPoint2 | Returns or sets the point on the second face. |
SegmentLength | Returns the linear dimension length indicates segment length for each weld. |
Spacing | Returns the linear dimension spacing indicates distance between each weld. |
StartDist | Returns the on path dimension start distance. |
StartVector | Returns or sets the start direction reversed or not. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ThroatThickToggle | Returns or sets the toggle throat thickness. |
ToggleCreateSkipWelds | Returns or sets the toggle to create skip welds. |
ToggleRecreateDeletedWelds | Returns or sets the toggle to recreate deleted welds. |
Uparameter1 | Returns or sets the u parameter for first face. |
Uparameter2 | Returns or sets the u parameter for second face. |
Vparameter1 | Returns or sets the v parameter for first face. |
Vparameter2 | Returns or sets the v parameter for second face. |
WeldingCharacteristics | Returns the welding characteristics. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FilletBuilderEnumConstructionMethod Enumeration | the options for which construction method to use. |
FilletBuilderEnumContour Enumeration | the Contour enum. |
FilletBuilderEnumExtendEdges Enumeration | the options for populating the edge selections. |
FilletBuilderEnumExtensionMethod Enumeration | the Extension enum. |
FilletBuilderEnumFillFaceHolesType Enumeration | the fill method to be applied. |
FilletBuilderEnumSkipWeldMethod Enumeration | the Skipweld enum. |
FilletBuilderEnumWeldingType Enumeration | the WeldingType enum. |
Property Detail¶
AddCosmeticEnd¶
-
FilletBuilder.
AddCosmeticEnd
¶ Returns or sets the value identify if a cosmtic end should be added to each end of the fillet.
-------------------------------------
Getter Method
Signature
AddCosmeticEnd
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddCosmeticEnd
Parameters: addCosmeticEnd (bool) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
AllowBroken¶
-
FilletBuilder.
AllowBroken
¶ Returns or sets the toggle to allow broken link.
-------------------------------------
Getter Method
Signature
AllowBroken
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowBroken
Parameters: allowBroken (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
AssignWeldPMI¶
-
FilletBuilder.
AssignWeldPMI
¶ Returns or sets the toggle to assign weld pmi.
-------------------------------------
Getter Method
Signature
AssignWeldPMI
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssignWeldPMI
Parameters: assignWeldPMI (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
Associative¶
-
FilletBuilder.
Associative
¶ Returns or sets the value identify if WAVE links should remain unbroken.
-------------------------------------
Getter Method
Signature
Associative
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative
Parameters: associative (bool) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
ConstructionMethod¶
-
FilletBuilder.
ConstructionMethod
¶ Returns or sets the value for determining the construction method.
Default method should be used for all conditions, unless you know the situation if for the roll around condition.
-------------------------------------
Getter Method
Signature
ConstructionMethod
Returns: Return type: NXOpen.Weld.FilletBuilderEnumConstructionMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstructionMethod
Parameters: constructionMethod ( NXOpen.Weld.FilletBuilderEnumConstructionMethod
) –New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
ContourHeight¶
-
FilletBuilder.
ContourHeight
¶ Returns the linear dimension contour height.
-------------------------------------
Getter Method
Signature
ContourHeight
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ContourType¶
-
FilletBuilder.
ContourType
¶ Returns or sets the contour.
-------------------------------------
Getter Method
Signature
ContourType
Returns: Return type: NXOpen.Weld.FilletBuilderEnumContour
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContourType
Parameters: contour ( NXOpen.Weld.FilletBuilderEnumContour
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DirectToggle¶
-
FilletBuilder.
DirectToggle
¶ Returns or sets the toggle to change direction.
-------------------------------------
Getter Method
Signature
DirectToggle
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectToggle
Parameters: directToggle (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DirectionVector1¶
-
FilletBuilder.
DirectionVector1
¶ Returns or sets the face normal direction.
-------------------------------------
Getter Method
Signature
DirectionVector1
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionVector1
Parameters: directionVector1 (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DirectionVector2¶
-
FilletBuilder.
DirectionVector2
¶ Returns or sets the face normal direction for the second face.
-------------------------------------
Getter Method
Signature
DirectionVector2
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionVector2
Parameters: directionVector2 (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DistTolerance¶
-
FilletBuilder.
DistTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistTolerance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistTolerance
Parameters: distTolerance (float) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
EdgeSet1¶
-
FilletBuilder.
EdgeSet1
¶ Returns the edge set1.
-------------------------------------
Getter Method
Signature
EdgeSet1
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
EdgeSet2¶
-
FilletBuilder.
EdgeSet2
¶ Returns the edge set2.
-------------------------------------
Getter Method
Signature
EdgeSet2
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
EndDist¶
-
FilletBuilder.
EndDist
¶ Returns the on path dimension end distance.
-------------------------------------
Getter Method
Signature
EndDist
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.0.0.
License requirements: None.
EndVector¶
-
FilletBuilder.
EndVector
¶ Returns or sets the end direction reversed or not.
-------------------------------------
Getter Method
Signature
EndVector
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndVector
Parameters: endVector (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
EnumMethod¶
-
FilletBuilder.
EnumMethod
¶ Returns or sets the enum method for skip welds.
-------------------------------------
Getter Method
Signature
EnumMethod
Returns: Return type: NXOpen.Weld.FilletBuilderEnumSkipWeldMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumMethod
Parameters: enumMethod ( NXOpen.Weld.FilletBuilderEnumSkipWeldMethod
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ExtendEdges¶
-
FilletBuilder.
ExtendEdges
¶ Returns or sets the value for how to populate the edge sets.
-------------------------------------
Getter Method
Signature
ExtendEdges
Returns: Return type: NXOpen.Weld.FilletBuilderEnumExtendEdges
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendEdges
Parameters: extendEdges ( NXOpen.Weld.FilletBuilderEnumExtendEdges
) –New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
ExtensionDistance¶
-
FilletBuilder.
ExtensionDistance
¶ Returns the linear dimension extension distance.
-------------------------------------
Getter Method
Signature
ExtensionDistance
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ExtensionMethod¶
-
FilletBuilder.
ExtensionMethod
¶ Returns or sets the extension method.
-------------------------------------
Getter Method
Signature
ExtensionMethod
Returns: Return type: NXOpen.Weld.FilletBuilderEnumExtensionMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtensionMethod
Parameters: extensionMethod ( NXOpen.Weld.FilletBuilderEnumExtensionMethod
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
FaceFillGapDistance¶
-
FilletBuilder.
FaceFillGapDistance
¶ Returns or sets the distance the fillet will span when there are gaps in the sheet definition.
-------------------------------------
Getter Method
Signature
FaceFillGapDistance
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceFillGapDistance
Parameters: faceFillGapDistance (float) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
FaceSet1¶
-
FilletBuilder.
FaceSet1
¶ Returns the face set1.
-------------------------------------
Getter Method
Signature
FaceSet1
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FaceSet2¶
-
FilletBuilder.
FaceSet2
¶ Returns the face set2.
-------------------------------------
Getter Method
Signature
FaceSet2
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FieldWeld¶
-
FilletBuilder.
FieldWeld
¶ Returns or sets the field weld.
-------------------------------------
Getter Method
Signature
FieldWeld
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FieldWeld
Parameters: fieldWeld (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
FillFaceHoles¶
-
FilletBuilder.
FillFaceHoles
¶ Returns or sets the value to identify if the face set should be filled during construction.
Only holes fully bounded by a single face will be filled.
-------------------------------------
Getter Method
Signature
FillFaceHoles
Returns: Return type: NXOpen.Weld.FilletBuilderEnumFillFaceHolesType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillFaceHoles
Parameters: fillFaceHolesType ( NXOpen.Weld.FilletBuilderEnumFillFaceHolesType
) –New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
FilletType¶
-
FilletBuilder.
FilletType
¶ Returns or sets the fillet type.
-------------------------------------
Getter Method
Signature
FilletType
Returns: Return type: NXOpen.Weld.FilletBuilderEnumWeldingType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FilletType
Parameters: filletType ( NXOpen.Weld.FilletBuilderEnumWeldingType
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
FirstLeg¶
-
FilletBuilder.
FirstLeg
¶ Returns the linear dimension first leg.
-------------------------------------
Getter Method
Signature
FirstLeg
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
NumberOfWelds¶
-
FilletBuilder.
NumberOfWelds
¶ Returns the expression number indicates number of welds in skip welds.
-------------------------------------
Getter Method
Signature
NumberOfWelds
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Pmi¶
-
FilletBuilder.
Pmi
¶ Returns or sets the pmi symbol.
-------------------------------------
Getter Method
Signature
Pmi
Returns: Return type: NXOpen.NXObject
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Pmi
Parameters: pmi ( NXOpen.NXObject
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SecondLeg¶
-
FilletBuilder.
SecondLeg
¶ Returns the linear dimension second leg.
-------------------------------------
Getter Method
Signature
SecondLeg
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SeedFace1¶
-
FilletBuilder.
SeedFace1
¶ Returns or sets the first seed face.
-------------------------------------
Getter Method
Signature
SeedFace1
Returns: Return type: NXOpen.Face
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedFace1
Parameters: seedFace1 ( NXOpen.Face
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SeedFace2¶
-
FilletBuilder.
SeedFace2
¶ Returns or sets the second seed face.
-------------------------------------
Getter Method
Signature
SeedFace2
Returns: Return type: NXOpen.Face
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedFace2
Parameters: seedFace2 ( NXOpen.Face
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SeedPoint1¶
-
FilletBuilder.
SeedPoint1
¶ Returns or sets the point on the first face.
-------------------------------------
Getter Method
Signature
SeedPoint1
Returns: Return type: NXOpen.Point3d
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedPoint1
Parameters: seedPoint1 ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SeedPoint2¶
-
FilletBuilder.
SeedPoint2
¶ Returns or sets the point on the second face.
-------------------------------------
Getter Method
Signature
SeedPoint2
Returns: Return type: NXOpen.Point3d
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedPoint2
Parameters: seedPoint1 ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SegmentLength¶
-
FilletBuilder.
SegmentLength
¶ Returns the linear dimension length indicates segment length for each weld.
-------------------------------------
Getter Method
Signature
SegmentLength
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Spacing¶
-
FilletBuilder.
Spacing
¶ Returns the linear dimension spacing indicates distance between each weld.
-------------------------------------
Getter Method
Signature
Spacing
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
StartDist¶
-
FilletBuilder.
StartDist
¶ Returns the on path dimension start distance.
-------------------------------------
Getter Method
Signature
StartDist
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.0.0.
License requirements: None.
StartVector¶
-
FilletBuilder.
StartVector
¶ Returns or sets the start direction reversed or not.
-------------------------------------
Getter Method
Signature
StartVector
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartVector
Parameters: startVector (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ThroatThickToggle¶
-
FilletBuilder.
ThroatThickToggle
¶ Returns or sets the toggle throat thickness.
-------------------------------------
Getter Method
Signature
ThroatThickToggle
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThroatThickToggle
Parameters: throatThickToggle (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ToggleCreateSkipWelds¶
-
FilletBuilder.
ToggleCreateSkipWelds
¶ Returns or sets the toggle to create skip welds.
-------------------------------------
Getter Method
Signature
ToggleCreateSkipWelds
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToggleCreateSkipWelds
Parameters: toggleCreateSkipWelds (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ToggleRecreateDeletedWelds¶
-
FilletBuilder.
ToggleRecreateDeletedWelds
¶ Returns or sets the toggle to recreate deleted welds.
-------------------------------------
Getter Method
Signature
ToggleRecreateDeletedWelds
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToggleRecreateDeletedWelds
Parameters: toggleRecreateDeletedWelds (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
Uparameter1¶
-
FilletBuilder.
Uparameter1
¶ Returns or sets the u parameter for first face.
-------------------------------------
Getter Method
Signature
Uparameter1
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Uparameter1
Parameters: u1 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
Uparameter2¶
-
FilletBuilder.
Uparameter2
¶ Returns or sets the u parameter for second face.
-------------------------------------
Getter Method
Signature
Uparameter2
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Uparameter2
Parameters: u2 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
Vparameter1¶
-
FilletBuilder.
Vparameter1
¶ Returns or sets the v parameter for first face.
-------------------------------------
Getter Method
Signature
Vparameter1
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vparameter1
Parameters: v1 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
Vparameter2¶
-
FilletBuilder.
Vparameter2
¶ Returns or sets the v parameter for second face.
-------------------------------------
Getter Method
Signature
Vparameter2
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vparameter2
Parameters: v2 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
WeldingCharacteristics¶
-
FilletBuilder.
WeldingCharacteristics
¶ Returns the welding characteristics.
-------------------------------------
Getter Method
Signature
WeldingCharacteristics
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FilletBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.