FilletBuilderEnumConstructionMethod Enumeration

NXOpen.Weld.FilletBuilder.EnumConstructionMethod is an alias for NXOpen.Weld.FilletBuilderEnumConstructionMethod

class NXOpen.Weld.FilletBuilderEnumConstructionMethod

Bases: object

the options for which construction method to use.

Enum Members

Enum Member Enum Member Description
Default
RollAround
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.