FilletBuilderEnumExtendEdges Enumeration

NXOpen.Weld.FilletBuilder.EnumExtendEdges is an alias for NXOpen.Weld.FilletBuilderEnumExtendEdges

class NXOpen.Weld.FilletBuilderEnumExtendEdges

Bases: object

the options for populating the edge selections.

Enum Members

Enum Member Enum Member Description
Manual
Automatic
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.