FeatureBuilder Class¶
-
class
NXOpen.Features.
FeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a Feature Builder to be used in the creation and modification of features.
Feature Builders manage the steps needed to correctly create features on a part.
This is an abstract class, and cannot be instantiated.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ParentFeatureInternal¶
-
FeatureBuilder.
ParentFeatureInternal
¶ Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal
-------------------------------------
Getter Method
Signature
ParentFeatureInternal
Returns: True = internal, False = external Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
-------------------------------------
Setter Method
Signature
ParentFeatureInternal
Parameters: isInternal (bool) – True = internal, False = external New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
PatchSolutionFlag¶
-
FeatureBuilder.
PatchSolutionFlag
¶ Returns or sets the patch solution flag
-------------------------------------
Getter Method
Signature
PatchSolutionFlag
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
PatchSolutionFlag
Parameters: optionValue (bool) – New in version NX8.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
PatchSurfaceFilename¶
-
FeatureBuilder.
PatchSurfaceFilename
¶ Returns or sets the patch surface filename
-------------------------------------
Getter Method
Signature
PatchSurfaceFilename
Returns: Return type: str New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
PatchSurfaceFilename
Parameters: surfaceFilename (str) – New in version NX8.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
SurroundingPatchSurfaceFilename¶
-
FeatureBuilder.
SurroundingPatchSurfaceFilename
¶ Returns or sets the surrounding patch surface filename
-------------------------------------
Getter Method
Signature
SurroundingPatchSurfaceFilename
Returns: Return type: str New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurroundingPatchSurfaceFilename
Parameters: surroundingSurfaceFilename (str) – New in version NX8.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Method Detail¶
CommitFeature¶
-
FeatureBuilder.
CommitFeature
¶ Commits the feature parameters and creates the feature
Signature
CommitFeature()
Returns: Return type: NXOpen.Features.Feature
New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
GetFeature¶
-
FeatureBuilder.
GetFeature
¶ Returns the feature currently being edited by this builder.
If a new feature is being created, and the builder has not yet been commited, returns None.
Signature
GetFeature()
Returns: Return type: NXOpen.Features.Feature
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
HideInternalParentFeatureAfterEdit¶
-
FeatureBuilder.
HideInternalParentFeatureAfterEdit
¶ Re-suppress an internal parent feature (a slave feature) after it has been edited.
Note that this method will do nothing if
ShowInternalParentFeatureForEdit()
has not previously been called. Also note that this action will happen automatically when the feature builder is destroyed so calling this method is not strictly necessary.Signature
HideInternalParentFeatureAfterEdit(parentFeature)
Parameters: parentFeature ( NXOpen.Features.Feature
) – Slave featureNew in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
SetParentFeatureInternal¶
-
FeatureBuilder.
SetParentFeatureInternal
¶ Overloaded method SetParentFeatureInternal
SetParentFeatureInternal(parentFeature)
ParentFeatureInternal
-------------------------------------
Set the parent features which would be internal or slaves to the feature being created or commited
Signature
SetParentFeatureInternal(parentFeature)
Parameters: parentFeature ( NXOpen.Features.Feature
) – Slave featureNew in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
-------------------------------------
Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal
-------------------------------------
Getter Method
Signature
ParentFeatureInternal
Parameters: isInternal (bool) – True = internal, False = external New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
-------------------------------------
Setter Method
Signature
ParentFeatureInternal
Parameters: isInternal (bool) – True = internal, False = external New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
-------------------------------------
ShowInternalParentFeatureForEdit¶
-
FeatureBuilder.
ShowInternalParentFeatureForEdit
¶ Unsuppress an internal parent feature (a slave feature) so it can be edited.
Signature
ShowInternalParentFeatureForEdit(parentFeature)
Parameters: parentFeature ( NXOpen.Features.Feature
) – Slave featureNew in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
UnsetParentFeatureInternal¶
-
FeatureBuilder.
UnsetParentFeatureInternal
¶ Set the internal parent feature of the feature being edited to external
Signature
UnsetParentFeatureInternal(parentFeature)
Parameters: parentFeature ( NXOpen.Features.Feature
) – Slave featureNew in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Validate¶
-
FeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.