ScCollector Class¶
-
class
NXOpen.
ScCollector
¶ Bases:
NXOpen.DisplayableObject
Represents a collector
ScCollector consists of collection of either faces, bodies, edges, curves or a mixed collection of these entities. The collection is defined by selection intent rules. Please refer documentation of
ScRuleFactory
for more details on available selection intent rules.ScRuleFactory
.To create a new instance of this class, use
NXOpen.ScCollectorCollection.CreateCollector()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddEvaluationFilter | Sets the evaluation filter on ScCollector |
Blank | Blanks the object. |
CopyCollector | Copy collector object |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Destroy | Destroy the ScCollector object |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMultiComponent | Gets the option set on ScCollector for collection from multiple components. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNonFeatureMode | Gets the option set on ScCollector for collection in non-feature mode. |
GetObjects | Returns the contents of a collector. |
GetObjectsSortedById | Returns the contents of a collector which are guaranteed to be sorted. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRules | Returns the rules of the a collector. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight | Highlights the object. |
IsEvaluationFilterEnabled | Checks whether the evaluation filter is present on ScCollector |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveEvaluationFilter | Removes the evaluation filter on ScCollector |
RemoveRule | Remove collector rule |
RemoveRules | Remove collector rules |
RemoveViewDependency | Remove dependency on all views from an object. |
ReplaceRules | Replace collector rules. |
SetAllowRefCurves | Sets whether to allow reference curves or not in the ScCollector |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetInterpart | Sets inter-part status |
SetMultiComponent | Sets the true option on ScCollector for collection from multiple components. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetNonFeatureMode | Sets the true option on ScCollector for collection in non-feature mode. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
IsOccurrence¶
-
ScCollector.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ScCollector.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ScCollector.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ScCollector.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ScCollector.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ScCollector.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddEvaluationFilter¶
-
ScCollector.
AddEvaluationFilter
¶ Sets the evaluation filter on ScCollector
Signature
AddEvaluationFilter(filterType)
Parameters: filterType ( NXOpen.ScEvaluationFiltertype
) – Enum ValueNew in version NX11.0.0.
License requirements: None.
CopyCollector¶
-
ScCollector.
CopyCollector
¶ Copy collector object
Signature
CopyCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
Destroy¶
-
ScCollector.
Destroy
¶ Destroy the ScCollector object
Signature
Destroy()
New in version NX5.0.0.
License requirements: None.
FindObject¶
-
ScCollector.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetMultiComponent¶
-
ScCollector.
GetMultiComponent
¶ Gets the option set on ScCollector for collection from multiple components.
A multi-component ScCollector can have collection from multiple components i.e., multiple parts or multiple instances of same part or both.
Signature
GetMultiComponent()
Returns: Multi-component option set on ScCollector Return type: bool New in version NX9.0.0.
License requirements: None.
GetNonFeatureMode¶
-
ScCollector.
GetNonFeatureMode
¶ Gets the option set on ScCollector for collection in non-feature mode.
An ScCollector in non-feature mode does not reference the feature data of the part from which the collection is done.
Signature
GetNonFeatureMode()
Returns: Non-feature mode set on ScCollector Return type: bool New in version NX9.0.0.
License requirements: None.
GetObjects¶
-
ScCollector.
GetObjects
¶ Returns the contents of a collector.
Signature
GetObjects()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX6.0.0.
License requirements: None.
GetObjectsSortedById¶
-
ScCollector.
GetObjectsSortedById
¶ Returns the contents of a collector which are guaranteed to be sorted.
Signature
GetObjectsSortedById()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX11.0.0.
License requirements: None.
GetRules¶
-
ScCollector.
GetRules
¶ Returns the rules of the a collector.
Signature
GetRules()
Returns: Selection intent rules. Return type: list of NXOpen.SelectionIntentRule
New in version NX6.0.0.
License requirements: None.
IsEvaluationFilterEnabled¶
-
ScCollector.
IsEvaluationFilterEnabled
¶ Checks whether the evaluation filter is present on ScCollector
Signature
IsEvaluationFilterEnabled(filterType)
Parameters: filterType ( NXOpen.ScEvaluationFiltertype
) – Enum ValueReturns: Return type: bool New in version NX11.0.0.
License requirements: None.
Print¶
-
ScCollector.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveEvaluationFilter¶
-
ScCollector.
RemoveEvaluationFilter
¶ Removes the evaluation filter on ScCollector
Signature
RemoveEvaluationFilter(filterType)
Parameters: filterType ( NXOpen.ScEvaluationFiltertype
) – Enum ValueNew in version NX11.0.0.
License requirements: None.
RemoveRule¶
-
ScCollector.
RemoveRule
¶ Remove collector rule
Signature
RemoveRule(ruleIndex)
Parameters: ruleIndex (int) – index (starting from 0) of the rule to be removed New in version NX7.0.0.
License requirements: None.
RemoveRules¶
-
ScCollector.
RemoveRules
¶ Remove collector rules
Signature
RemoveRules(rules)
Parameters: rules (list of NXOpen.SelectionIntentRule
) – Selection intent rules to be removedNew in version NX8.0.0.
License requirements: None.
ReplaceRules¶
-
ScCollector.
ReplaceRules
¶ Overloaded method ReplaceRules
ReplaceRules(rules, createRulesWoUpdate)
ReplaceRules(rules, negatedEntities, createRulesWoUpdate)
-------------------------------------
Replace collector rules.
Signature
ReplaceRules(rules, createRulesWoUpdate)
Parameters: - rules (list of
NXOpen.SelectionIntentRule
) – Selection intent rules. To create selection intent rules see documentation ofScRuleFactory
for more details. - createRulesWoUpdate (bool) – Flag to tell whether rules should be created wo_update
New in version NX4.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Replace collector rules and specify negated entities.
Signature
ReplaceRules(rules, negatedEntities, createRulesWoUpdate)
Parameters: - rules (list of
NXOpen.SelectionIntentRule
) – Selection intent rules. To create selection intent rules see documentation ofScRuleFactory
for more details. - negatedEntities (list of
NXOpen.DisplayableObject
) – Entities in the rules that should be removed from the collector. - createRulesWoUpdate (bool) – Flag to tell whether rules should be created wo_update
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
SetAllowRefCurves¶
-
ScCollector.
SetAllowRefCurves
¶ Sets whether to allow reference curves or not in the ScCollector
Signature
SetAllowRefCurves(allowRefCurves)
Parameters: allowRefCurves (bool) – True to allow reference curves in ScCollector New in version NX11.0.2.
License requirements: None.
SetInterpart¶
-
ScCollector.
SetInterpart
¶ Sets inter-part status
This function sets the value of interpart flag on ScCollector. Error will be raised while setting this option on ScCollector in following conditions: (1) ScCollector is NULL. (2) ScCollector object is not of SC_collector class. (3) ScCollector is of hybrid part option. (4) Multi-component option is already set on ScCollector.
Signature
SetInterpart(interpart)
Parameters: interpart (bool) – True to set collector as interpart New in version NX6.0.0.
License requirements: None.
SetMultiComponent¶
-
ScCollector.
SetMultiComponent
¶ Sets the true option on ScCollector for collection from multiple components.
A multi-component ScCollector can have collection from multiple components i.e., multiple parts or multiple instances of same part or both. This method should be used only if such collection is desired. Error will be raised while setting this option on ScCollector in following conditions: (1) Inter-part option is already set on ScCollector.
Signature
SetMultiComponent()
New in version NX9.0.0.
License requirements: None.
SetName¶
-
ScCollector.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetNonFeatureMode¶
-
ScCollector.
SetNonFeatureMode
¶ Sets the true option on ScCollector for collection in non-feature mode.
An ScCollector in non-feature mode does not reference the feature data of the part from which the collection is done. The option should be set on an empty ScCollector only. For a non-empty ScCollector, setting this option will raise error in following conditions: (1) ScCollector is referencing feature data and non-feature mode is set true. (2) ScCollector is not referencing feature data and non-feature mode is set false.
Signature
SetNonFeatureMode()
New in version NX9.0.0.
License requirements: None.