FilletBuilderEnumSkipWeldMethod Enumeration

NXOpen.Weld.FilletBuilder.EnumSkipWeldMethod is an alias for NXOpen.Weld.FilletBuilderEnumSkipWeldMethod

class NXOpen.Weld.FilletBuilderEnumSkipWeldMethod

Bases: object

the Skipweld enum.

Enum Members

Enum Member Enum Member Description
NumberLength
NumberSpacing
SpacingLength
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.