OnPathDimensionBuilder Class¶
-
class
NXOpen.GeometricUtilities.
OnPathDimensionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Builds an on-path dimension
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Expression | Returns the expression for the value of the dimension |
IsFlipped | Returns or sets a flag indicating whether the length along the path is evaluated starting from the end point of path instead of the start point of the path |
IsParameterUsed | Returns or sets a flag indicating whether the expression is in terms of the mathematical parameter of the path (is_parameter_used = true) or in terms of its arclength (is_parameter_used = false). |
IsPercentUsed | Returns or sets a flag indicating whether the expression represents the percentage along the path. |
Path | Returns the path that the dimension is evaluated on. |
Tag | Returns the Tag for this object. |
ThroughPoint | Returns or sets the through point |
Methods¶
Method | Description |
---|---|
Update | Updates this object if the path or through point location has changed. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OnPathDimensionBuilderUpdateReason Enumeration | The type of update to perform |
Property Detail¶
Expression¶
-
OnPathDimensionBuilder.
Expression
¶ Returns the expression for the value of the dimension
-------------------------------------
Getter Method
Signature
Expression
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
IsFlipped¶
-
OnPathDimensionBuilder.
IsFlipped
¶ Returns or sets a flag indicating whether the length along the path is evaluated starting from the end point of path instead of the start point of the path
-------------------------------------
Getter Method
Signature
IsFlipped
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsFlipped
Parameters: flipped (bool) – New in version NX5.0.0.
License requirements: None.
IsParameterUsed¶
-
OnPathDimensionBuilder.
IsParameterUsed
¶ Returns or sets a flag indicating whether the expression is in terms of the mathematical parameter of the path (is_parameter_used = true) or in terms of its arclength (is_parameter_used = false).
When value is true, the value will always be expressed in terms of percentage (between 0 and 100) regardless of is_percent_used’s setting. This property must be used with care. Most referencing classes will only accept arclength values, and setting this property to true for those classes will result in a run time error. Consult the referencing class documentation to see if this value can be true for that particular operation.
-------------------------------------
Getter Method
Signature
IsParameterUsed
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsParameterUsed
Parameters: useParameter (bool) – New in version NX5.0.0.
License requirements: None.
IsPercentUsed¶
-
OnPathDimensionBuilder.
IsPercentUsed
¶ Returns or sets a flag indicating whether the expression represents the percentage along the path.
If false, the expression represents the length along the path
-------------------------------------
Getter Method
Signature
IsPercentUsed
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsPercentUsed
Parameters: usePercent (bool) – New in version NX5.0.0.
License requirements: None.
Path¶
-
OnPathDimensionBuilder.
Path
¶ Returns the path that the dimension is evaluated on.
Note: in some cases, the builder will not permit you to change the path
-------------------------------------
Getter Method
Signature
Path
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
ThroughPoint¶
-
OnPathDimensionBuilder.
ThroughPoint
¶ Returns or sets the through point
-------------------------------------
Getter Method
Signature
ThroughPoint
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThroughPoint
Parameters: throughPoint ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
Update¶
-
OnPathDimensionBuilder.
Update
¶ Updates this object if the path or through point location has changed.
Call this function if the path is a section and you have added or removed curves from the section, or if there is a through point and the coordinates of the through point have changed.
Signature
Update(updateReason)
Parameters: updateReason ( NXOpen.GeometricUtilities.OnPathDimensionBuilderUpdateReason
) –New in version NX5.0.0.
License requirements: None.
Validate¶
-
OnPathDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.