OnPathDimensionBuilderUpdateReason Enumeration¶
NXOpen.GeometricUtilities.OnPathDimensionBuilder.UpdateReason is an alias for NXOpen.GeometricUtilities.OnPathDimensionBuilderUpdateReason
-
class
NXOpen.GeometricUtilities.
OnPathDimensionBuilderUpdateReason
¶ Bases:
object
The type of update to perform
Enum Members
Enum Member Enum Member Description Path Update because of the path may have changed ThroughPoint Update because the through point location may have changed All Update because either path or through point location may have changed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-