Face Class¶
-
class
NXOpen.
Face
¶ Bases:
NXOpen.DisplayableObject
,NXOpen.ISurface
,NXOpen.IReferenceAxis
,NXOpen.IProfile
,NXOpen.IOrientation
,NXOpen.IParameterizedSurface
Represents a face
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
SolidFaceType | Returns the Parasolid type of the face |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DestroyOwnedFacets | Destroys all IFacet objects owned by this face. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBody | Returns the body containing this face |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetEdges | Returns the edges in the face |
GetFirstFacetOnFace | Returns first facet on convergent face. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextFacet | Returns a facet next to the input facet on a convergent face. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNumberOfFacets | Returns the number of facets on a convergent face. |
GetNumberOfVertices | Returns the number of vertices on this convergent face. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUnsortedEdges | Returns the edges in the face |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Enumerations¶
FaceFaceType Enumeration | Solid face type. |
Property Detail¶
IsOccurrence¶
-
Face.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Face.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Face.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Face.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Face.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Face.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SolidFaceType¶
-
Face.
SolidFaceType
¶ Returns the Parasolid type of the face
-------------------------------------
Getter Method
Signature
SolidFaceType
Returns: Return type: NXOpen.FaceFaceType
New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
DestroyOwnedFacets¶
-
Face.
DestroyOwnedFacets
¶ Destroys all
IFacet
objects owned by this face.Please note that this method does not geometrically delete a facet from its surface mesh leaving a hole. It only deletes the tagged object created to represent the individual facet.
Signature
DestroyOwnedFacets()
New in version NX12.0.0.
License requirements: None.
FindObject¶
-
Face.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetBody¶
-
Face.
GetBody
¶ Returns the body containing this face
Signature
GetBody()
Returns: Return type: NXOpen.Body
New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetEdges¶
-
Face.
GetEdges
¶ Returns the edges in the face
The edges are sorted according to the journal identifier of the edge.
Signature
GetEdges()
Returns: Return type: list of NXOpen.Edge
New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetFirstFacetOnFace¶
-
Face.
GetFirstFacetOnFace
¶ Returns first facet on convergent face.
This method is valid only for convergent faces. If this face is not a convergent face, then an error is returned.
Signature
GetFirstFacetOnFace()
Returns: the first facet on a face. Return type: NXOpen.ConvergentFacet
New in version NX11.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetNextFacet¶
-
Face.
GetNextFacet
¶ Returns a facet next to the input facet on a convergent face.
Note that, the next facet is the facet immediately next to the given facet in an internal ordered sequence of facets. It is not necessarily adjacent to the given facet. If the input facet is the last facet on the face, then None is returned. This method is valid only for convergent faces. If this face is not a convergent face, then an error is returned.
Signature
GetNextFacet(inputFacet)
Parameters: inputFacet ( NXOpen.ConvergentFacet
) – the input facet, next to which facet is to find.Returns: the next facet. Return type: NXOpen.ConvergentFacet
New in version NX11.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetNumberOfFacets¶
-
Face.
GetNumberOfFacets
¶ Returns the number of facets on a convergent face.
This method is valid only for convergent faces. If this face is not a convergent face, then an error is returned
Signature
GetNumberOfFacets()
Returns: the number of facets on a face Return type: int New in version NX11.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetNumberOfVertices¶
-
Face.
GetNumberOfVertices
¶ Returns the number of vertices on this convergent face.
This method is valid only for convergent faces. If this face is not a convergent face, then an error is returned.
Signature
GetNumberOfVertices()
Returns: the number of vertices on a face Return type: int New in version NX11.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetUnsortedEdges¶
-
Face.
GetUnsortedEdges
¶ Returns the edges in the face
The edges returned from this method are in no guaranteed order. This method will be faster than
NXOpen.Face.GetEdges()
.Signature
GetUnsortedEdges()
Returns: Return type: list of NXOpen.Edge
New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Print¶
-
Face.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
Face.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.