FaceFaceType Enumeration¶
NXOpen.Face.FaceType is an alias for NXOpen.FaceFaceType
-
class
NXOpen.
FaceFaceType
¶ Bases:
object
Solid face type.
Enum Members
Enum Member Enum Member Description Rubber Rubber face, no surface attached Planar Planar face Cylindrical Cylindrical face Conical Conical face Spherical Spherical face SurfaceOfRevolution Face from surface of revolution Parametric Parametric face Blending Blending face Offset Offset face Swept Swept face Convergent Convergent face Undefined Undefined face type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-