FilletBuilderEnumExtensionMethod Enumeration

NXOpen.Weld.FilletBuilder.EnumExtensionMethod is an alias for NXOpen.Weld.FilletBuilderEnumExtensionMethod

class NXOpen.Weld.FilletBuilderEnumExtensionMethod

Bases: object

the Extension enum.

Enum Members

Enum Member Enum Member Description
Automatic
ByValue
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.