FilletBuilderEnumFillFaceHolesType Enumeration¶
NXOpen.Weld.FilletBuilder.EnumFillFaceHolesType is an alias for NXOpen.Weld.FilletBuilderEnumFillFaceHolesType
-
class
NXOpen.Weld.
FilletBuilderEnumFillFaceHolesType
¶ Bases:
object
the fill method to be applied.
Enum Members
Enum Member Enum Member Description NotSet Set1 Set2 Both -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-