StudioXformBuilder Class¶
-
class
NXOpen.Features.
StudioXformBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.StudioXform
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateStudioXformBuilder()
Default values.
Property Value AdvancedMethod AdvanceOff CurveRange.AnchorPosition Start DegreesAndSegmentsOrPatches.Degree 3 DegreesAndSegmentsOrPatches.SegmentsOrPatches 1 DegreesAndSegmentsOrPatches.UDegree 5 DegreesAndSegmentsOrPatches.UPatches 1 DegreesAndSegmentsOrPatches.VDegree 5 DegreesAndSegmentsOrPatches.VPatches 1 FallOffScale 0 FeatureSaveMethod Relative InsertKnotDirection UDirection InsertKnotParameter 20 IsSingleSelection 1 KeepAllContinuity 0 LockRegionUEndFlexibility 0 LockRegionUStartFlexibility 0 LockRegionVEndFlexibility 0 LockRegionVStartFlexibility 0 PlanarizeDirection U PlanarizeMethod AtPlaneLocation PlanarizePlaneOption YcZc ProportionalAllU 0 ProportionalAllV 0 ProportionalFallOffScale 0 ProportionalMoveAfterU 0 ProportionalMoveAfterV 0 ProportionalMoveBeforeU 0 ProportionalMoveBeforeV 0 RotationDirection Zc ScalingDirection Zc SurfaceRange.AnchorPosition Vertex1 TranslationDirection Zc New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Features.StudioXformBuilderEx
instead.
Properties¶
Property | Description |
---|---|
AdvancedMethod | Returns or sets the advanced method |
CenterPoint | Returns or sets the scaling center type |
ContinuityUMax | Returns the continuity at U maximum |
ContinuityUMin | Returns the continuity at U minimum |
ContinuityVMax | Returns the continuity at V maximum |
ContinuityVMin | Returns the continuity at V minimum |
ControlPoleManager | Returns the control pole manager |
CurveRange | Returns the curve range |
DegreesAndSegmentsOrPatches | Returns the degrees and segments or patches |
FallOffScale | Returns or sets the fall off scale |
FeatureSaveMethod | Returns or sets the feature save method |
InsertKnotDirection | Returns or sets the insert knot direction |
InsertKnotParameter | Returns or sets the parameter where to insert knots |
IsSingleSelection | Returns or sets the single selection flag |
KeepAllContinuity | Returns or sets a value indicating whether to keep all continuity |
LockRegionUEndFlexibility | Returns or sets the lock region flexibility at U end |
LockRegionUStartFlexibility | Returns or sets the lock region flexibility at U start |
LockRegionVEndFlexibility | Returns or sets the lock region flexibility at V end |
LockRegionVStartFlexibility | Returns or sets the lock region flexibility at V start |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PivotPoint | Returns or sets the rotating center |
PlanarizeArbitraryPlane | Returns or sets the planarize arbitrary plane |
PlanarizeDirection | Returns or sets the planarize direction |
PlanarizeMethod | Returns or sets the planarize method |
PlanarizePlaneOption | Returns or sets the planarize plane option |
ProportionalAllU | Returns or sets a value indicating whether to use all poles in U direction during the proportional movement |
ProportionalAllV | Returns or sets a value indicating whether to use all poles in V direction during the proportional movement |
ProportionalFallOffScale | Returns or sets the proportional fall off scale |
ProportionalMoveAfterU | Returns or sets a value indicating the pole number after u to participate in the proportional movement |
ProportionalMoveAfterV | Returns or sets a value indicating the pole number after v to participate in the proportional movement |
ProportionalMoveBeforeU | Returns or sets a value indicating the pole number before u to participate in the proportional movement |
ProportionalMoveBeforeV | Returns or sets a value indicating the pole number before v to participate in the proportional movement |
RotatingPivot | Returns or sets the rotating center type |
RotationArbitraryPlane | Returns or sets the rotation arbitrary plane. |
RotationArbitraryVector | Returns or sets the rotation arbitrary vector. |
RotationDirection | Returns or sets the rotation direction |
ScalingArbitraryPlane | Returns or sets the scaling arbitrary plane. |
ScalingArbitraryVector | Returns or sets the scaling arbitrary vector. |
ScalingCenter | Returns or sets the scaling center |
ScalingDirection | Returns or sets the scaling direction |
SurfaceRange | Returns the surface range |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TranslationArbitraryPlane | Returns or sets the translation arbitrary plane. |
TranslationArbitraryVector | Returns or sets the translation arbitrary vector. |
TranslationDirection | Returns or sets the translation direction |
Type | Returns or sets the type |
XformObjects | Returns the object to be transformed. |
Methods¶
Method | Description |
---|---|
ChangeDegree | Changes degree of the selected xform object |
ChangeFlexibility | Changes flexibility of the selected xform object |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
ConvertParameters | Converts parameters of the feature that owns selected xform object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FallOffReset | Reset the fall off scale |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
InsertKnot | Inserts knot in the selected xform object |
InsertKnots | Insert knots |
ProportionalReset | Reset the proportional scale |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShapeReset | Reset the shape of a edited face or curve |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateLockRegionGeometry | Update lock region geometry with current geometry |
UpdateXformObject | Updates the selected xform object |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AdvancedMethod¶
-
StudioXformBuilder.
AdvancedMethod
¶ Returns or sets the advanced method
-------------------------------------
Getter Method
Signature
AdvancedMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderAdvancedMethodType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvancedMethod(advancedMethod)
Parameters: advancedMethod ( NXOpen.Features.StudioXformBuilderAdvancedMethodType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CenterPoint¶
-
StudioXformBuilder.
CenterPoint
¶ Returns or sets the scaling center type
-------------------------------------
Getter Method
Signature
CenterPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPoint(centerPoint)
Parameters: centerPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ContinuityUMax¶
-
StudioXformBuilder.
ContinuityUMax
¶ Returns the continuity at U maximum
-------------------------------------
Getter Method
Signature
ContinuityUMax()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ContinuityUMin¶
-
StudioXformBuilder.
ContinuityUMin
¶ Returns the continuity at U minimum
-------------------------------------
Getter Method
Signature
ContinuityUMin()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ContinuityVMax¶
-
StudioXformBuilder.
ContinuityVMax
¶ Returns the continuity at V maximum
-------------------------------------
Getter Method
Signature
ContinuityVMax()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ContinuityVMin¶
-
StudioXformBuilder.
ContinuityVMin
¶ Returns the continuity at V minimum
-------------------------------------
Getter Method
Signature
ContinuityVMin()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: None.
ControlPoleManager¶
-
StudioXformBuilder.
ControlPoleManager
¶ Returns the control pole manager
-------------------------------------
Getter Method
Signature
ControlPoleManager()
Returns: Return type: NXOpen.GeometricUtilities.ControlPoleManagerData
New in version NX6.0.0.
License requirements: None.
CurveRange¶
-
StudioXformBuilder.
CurveRange
¶ Returns the curve range
-------------------------------------
Getter Method
Signature
CurveRange()
Returns: Return type: NXOpen.GeometricUtilities.CurveRangeBuilder
New in version NX6.0.0.
License requirements: None.
DegreesAndSegmentsOrPatches¶
-
StudioXformBuilder.
DegreesAndSegmentsOrPatches
¶ Returns the degrees and segments or patches
-------------------------------------
Getter Method
Signature
DegreesAndSegmentsOrPatches()
Returns: Return type: NXOpen.GeometricUtilities.DegreesAndSegmentsOrPatchesBuilder
New in version NX6.0.0.
License requirements: None.
FallOffScale¶
-
StudioXformBuilder.
FallOffScale
¶ Returns or sets the fall off scale
-------------------------------------
Getter Method
Signature
FallOffScale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FallOffScale(fallOffScale)
Parameters: fallOffScale (float) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FeatureSaveMethod¶
-
StudioXformBuilder.
FeatureSaveMethod
¶ Returns or sets the feature save method
-------------------------------------
Getter Method
Signature
FeatureSaveMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderFeatureType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureSaveMethod(featureSaveMethod)
Parameters: featureSaveMethod ( NXOpen.Features.StudioXformBuilderFeatureType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnotDirection¶
-
StudioXformBuilder.
InsertKnotDirection
¶ Returns or sets the insert knot direction
-------------------------------------
Getter Method
Signature
InsertKnotDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderInsertKnotDirectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertKnotDirection(insertKnotDirection)
Parameters: insertKnotDirection ( NXOpen.Features.StudioXformBuilderInsertKnotDirectionType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnotParameter¶
-
StudioXformBuilder.
InsertKnotParameter
¶ Returns or sets the parameter where to insert knots
-------------------------------------
Getter Method
Signature
InsertKnotParameter()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertKnotParameter(insertKnotSlider)
Parameters: insertKnotSlider (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
IsSingleSelection¶
-
StudioXformBuilder.
IsSingleSelection
¶ Returns or sets the single selection flag
-------------------------------------
Getter Method
Signature
IsSingleSelection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSingleSelection(singleSelectionFlag)
Parameters: singleSelectionFlag (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
KeepAllContinuity¶
-
StudioXformBuilder.
KeepAllContinuity
¶ Returns or sets a value indicating whether to keep all continuity
-------------------------------------
Getter Method
Signature
KeepAllContinuity()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepAllContinuity(keepAllContinuity)
Parameters: keepAllContinuity (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionUEndFlexibility¶
-
StudioXformBuilder.
LockRegionUEndFlexibility
¶ Returns or sets the lock region flexibility at U end
-------------------------------------
Getter Method
Signature
LockRegionUEndFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionUEndFlexibility(lockRegionUEndFlexibility)
Parameters: lockRegionUEndFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionUStartFlexibility¶
-
StudioXformBuilder.
LockRegionUStartFlexibility
¶ Returns or sets the lock region flexibility at U start
-------------------------------------
Getter Method
Signature
LockRegionUStartFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionUStartFlexibility(lockRegionUStartFlexibility)
Parameters: lockRegionUStartFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionVEndFlexibility¶
-
StudioXformBuilder.
LockRegionVEndFlexibility
¶ Returns or sets the lock region flexibility at V end
-------------------------------------
Getter Method
Signature
LockRegionVEndFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionVEndFlexibility(lockRegionVEndFlexibility)
Parameters: lockRegionVEndFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LockRegionVStartFlexibility¶
-
StudioXformBuilder.
LockRegionVStartFlexibility
¶ Returns or sets the lock region flexibility at V start
-------------------------------------
Getter Method
Signature
LockRegionVStartFlexibility()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockRegionVStartFlexibility(lockRegionVStartFlexibility)
Parameters: lockRegionVStartFlexibility (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PivotPoint¶
-
StudioXformBuilder.
PivotPoint
¶ Returns or sets the rotating center
-------------------------------------
Getter Method
Signature
PivotPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PivotPoint(pivotPoint)
Parameters: pivotPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizeArbitraryPlane¶
-
StudioXformBuilder.
PlanarizeArbitraryPlane
¶ Returns or sets the planarize arbitrary plane
-------------------------------------
Getter Method
Signature
PlanarizeArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizeArbitraryPlane(planarizeArbitraryPlane)
Parameters: planarizeArbitraryPlane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizeDirection¶
-
StudioXformBuilder.
PlanarizeDirection
¶ Returns or sets the planarize direction
-------------------------------------
Getter Method
Signature
PlanarizeDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderPlanarizeDirectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizeDirection(planarizeDirection)
Parameters: planarizeDirection ( NXOpen.Features.StudioXformBuilderPlanarizeDirectionType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizeMethod¶
-
StudioXformBuilder.
PlanarizeMethod
¶ Returns or sets the planarize method
-------------------------------------
Getter Method
Signature
PlanarizeMethod()
Returns: Return type: NXOpen.Features.StudioXformBuilderPlanarizeMethodType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizeMethod(planarizeMethod)
Parameters: planarizeMethod ( NXOpen.Features.StudioXformBuilderPlanarizeMethodType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
PlanarizePlaneOption¶
-
StudioXformBuilder.
PlanarizePlaneOption
¶ Returns or sets the planarize plane option
-------------------------------------
Getter Method
Signature
PlanarizePlaneOption()
Returns: Return type: NXOpen.Features.StudioXformBuilderPlanarizePlaneOptionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlanarizePlaneOption(planarizePlaneOption)
Parameters: planarizePlaneOption ( NXOpen.Features.StudioXformBuilderPlanarizePlaneOptionType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalAllU¶
-
StudioXformBuilder.
ProportionalAllU
¶ Returns or sets a value indicating whether to use all poles in U direction during the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalAllU()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalAllU(proportionalAllU)
Parameters: proportionalAllU (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalAllV¶
-
StudioXformBuilder.
ProportionalAllV
¶ Returns or sets a value indicating whether to use all poles in V direction during the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalAllV()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalAllV(proportionalAllV)
Parameters: proportionalAllV (bool) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalFallOffScale¶
-
StudioXformBuilder.
ProportionalFallOffScale
¶ Returns or sets the proportional fall off scale
-------------------------------------
Getter Method
Signature
ProportionalFallOffScale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalFallOffScale(proportionalFallOffScale)
Parameters: proportionalFallOffScale (float) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveAfterU¶
-
StudioXformBuilder.
ProportionalMoveAfterU
¶ Returns or sets a value indicating the pole number after u to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveAfterU()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveAfterU(proportionalMoveAfterU)
Parameters: proportionalMoveAfterU (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveAfterV¶
-
StudioXformBuilder.
ProportionalMoveAfterV
¶ Returns or sets a value indicating the pole number after v to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveAfterV()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveAfterV(proportionalMoveAfterV)
Parameters: proportionalMoveAfterV (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveBeforeU¶
-
StudioXformBuilder.
ProportionalMoveBeforeU
¶ Returns or sets a value indicating the pole number before u to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveBeforeU()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveBeforeU(proportionalMoveBeforeU)
Parameters: proportionalMoveBeforeU (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalMoveBeforeV¶
-
StudioXformBuilder.
ProportionalMoveBeforeV
¶ Returns or sets a value indicating the pole number before v to participate in the proportional movement
-------------------------------------
Getter Method
Signature
ProportionalMoveBeforeV()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProportionalMoveBeforeV(proportionalMoveBeforeV)
Parameters: proportionalMoveBeforeV (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotatingPivot¶
-
StudioXformBuilder.
RotatingPivot
¶ Returns or sets the rotating center type
-------------------------------------
Getter Method
Signature
RotatingPivot()
Returns: Return type: NXOpen.Features.StudioXformBuilderRotatingPivotType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotatingPivot(rotatePivot)
Parameters: rotatePivot ( NXOpen.Features.StudioXformBuilderRotatingPivotType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotationArbitraryPlane¶
-
StudioXformBuilder.
RotationArbitraryPlane
¶ Returns or sets the rotation arbitrary plane.
Used only when the RotationPlane is ArbitraryPlane.
-------------------------------------
Getter Method
Signature
RotationArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationArbitraryPlane(rotateArbitraryPlane)
Parameters: rotateArbitraryPlane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotationArbitraryVector¶
-
StudioXformBuilder.
RotationArbitraryVector
¶ Returns or sets the rotation arbitrary vector.
Used only when the RotationDirection is ArbitraryDirection.
-------------------------------------
Getter Method
Signature
RotationArbitraryVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationArbitraryVector(rotateArbitraryVector)
Parameters: rotateArbitraryVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RotationDirection¶
-
StudioXformBuilder.
RotationDirection
¶ Returns or sets the rotation direction
-------------------------------------
Getter Method
Signature
RotationDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderRotationDirectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationDirection(rotateDirection)
Parameters: rotateDirection ( NXOpen.Features.StudioXformBuilderRotationDirectionType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingArbitraryPlane¶
-
StudioXformBuilder.
ScalingArbitraryPlane
¶ Returns or sets the scaling arbitrary plane.
Used only when the ScalingDirection is ArbitraryPlane.
-------------------------------------
Getter Method
Signature
ScalingArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingArbitraryPlane(scaleArbitraryPlane)
Parameters: scaleArbitraryPlane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingArbitraryVector¶
-
StudioXformBuilder.
ScalingArbitraryVector
¶ Returns or sets the scaling arbitrary vector.
Used only when the ScalingDirection is ArbitraryDirection.
-------------------------------------
Getter Method
Signature
ScalingArbitraryVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingArbitraryVector(scaleArbitraryVector)
Parameters: scaleArbitraryVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingCenter¶
-
StudioXformBuilder.
ScalingCenter
¶ Returns or sets the scaling center
-------------------------------------
Getter Method
Signature
ScalingCenter()
Returns: Return type: NXOpen.Features.StudioXformBuilderScalingCenterType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingCenter(scaleCenter)
Parameters: scaleCenter ( NXOpen.Features.StudioXformBuilderScalingCenterType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ScalingDirection¶
-
StudioXformBuilder.
ScalingDirection
¶ Returns or sets the scaling direction
-------------------------------------
Getter Method
Signature
ScalingDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderScalingDirectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingDirection(scaleDirection)
Parameters: scaleDirection ( NXOpen.Features.StudioXformBuilderScalingDirectionType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SurfaceRange¶
-
StudioXformBuilder.
SurfaceRange
¶ Returns the surface range
-------------------------------------
Getter Method
Signature
SurfaceRange()
Returns: Return type: NXOpen.GeometricUtilities.SurfaceRangeBuilder
New in version NX6.0.0.
License requirements: None.
TranslationArbitraryPlane¶
-
StudioXformBuilder.
TranslationArbitraryPlane
¶ Returns or sets the translation arbitrary plane.
Used only when the TranslationDirection is ArbitraryPlane.
-------------------------------------
Getter Method
Signature
TranslationArbitraryPlane()
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TranslationArbitraryPlane(translateArbitraryPlane)
Parameters: translateArbitraryPlane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
TranslationArbitraryVector¶
-
StudioXformBuilder.
TranslationArbitraryVector
¶ Returns or sets the translation arbitrary vector.
Used only when the TranslationDirection is ArbitraryDirection.
-------------------------------------
Getter Method
Signature
TranslationArbitraryVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TranslationArbitraryVector(translateArbitraryVector)
Parameters: translateArbitraryVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
TranslationDirection¶
-
StudioXformBuilder.
TranslationDirection
¶ Returns or sets the translation direction
-------------------------------------
Getter Method
Signature
TranslationDirection()
Returns: Return type: NXOpen.Features.StudioXformBuilderTranslationDirectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TranslationDirection(translateDirection)
Parameters: translateDirection ( NXOpen.Features.StudioXformBuilderTranslationDirectionType
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Type¶
-
StudioXformBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.StudioXformBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.StudioXformBuilderTypes
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
XformObjects¶
-
StudioXformBuilder.
XformObjects
¶ Returns the object to be transformed.
Any face having b-surface type geometry or curve having b-curve geometry can be transformed.
-------------------------------------
Getter Method
Signature
XformObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
ChangeDegree¶
-
StudioXformBuilder.
ChangeDegree
¶ Changes degree of the selected xform object
Signature
ChangeDegree(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to change degree ofNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ChangeFlexibility¶
-
StudioXformBuilder.
ChangeFlexibility
¶ Changes flexibility of the selected xform object
Signature
ChangeFlexibility(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to change flexibility ofNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ConvertParameters¶
-
StudioXformBuilder.
ConvertParameters
¶ Converts parameters of the feature that owns selected xform object.
Converts through points studio spline feature to by poles feature, otherwise removes parameters of the feature.
Signature
ConvertParameters(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to convert pameters fromNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FallOffReset¶
-
StudioXformBuilder.
FallOffReset
¶ Reset the fall off scale
Signature
FallOffReset()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnot¶
-
StudioXformBuilder.
InsertKnot
¶ Inserts knot in the selected xform object
Signature
InsertKnot(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to insert knot inNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InsertKnots¶
-
StudioXformBuilder.
InsertKnots
¶ Insert knots
Signature
InsertKnots()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProportionalReset¶
-
StudioXformBuilder.
ProportionalReset
¶ Reset the proportional scale
Signature
ProportionalReset()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ShapeReset¶
-
StudioXformBuilder.
ShapeReset
¶ Reset the shape of a edited face or curve
Signature
ShapeReset()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
UpdateLockRegionGeometry¶
-
StudioXformBuilder.
UpdateLockRegionGeometry
¶ Update lock region geometry with current geometry
Signature
UpdateLockRegionGeometry(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to change flexibility ofNew in version NX6.0.2.
License requirements: studio_free_form (“STUDIO FREE FORM”)
UpdateXformObject¶
-
StudioXformBuilder.
UpdateXformObject
¶ Updates the selected xform object
Signature
UpdateXformObject(xformObject)
Parameters: xformObject ( NXOpen.NXObject
) – the selected face or curve to be editedNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
StudioXformBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.