StudioXformBuilderScalingCenterType Enumeration¶
NXOpen.Features.StudioXformBuilder.ScalingCenterType is an alias for NXOpen.Features.StudioXformBuilderScalingCenterType
-
class
NXOpen.Features.
StudioXformBuilderScalingCenterType
¶ Bases:
object
Represents the scaling center type
Enum Members
Enum Member Enum Member Description AboutObjectCenter Scale center at the object centerAboutSelectedObject Scale center at the selected objectAboutPoint Scale center at a point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-