StudioXformBuilderScalingDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilder.ScalingDirectionType is an alias for NXOpen.Features.StudioXformBuilderScalingDirectionType
-
class
NXOpen.Features.
StudioXformBuilderScalingDirectionType
¶ Bases:
object
Represents the scaling direction type
Enum Members
Enum Member Enum Member Description ScaleUniformly Scale uniformlyPlaneOfCurve Scale on Plane of curveXc Scale in X directionYc Scale in Y directionZc Scale in Z directionYcZc Scale on Y-Z planeXcZc Scale on X-Z planeXcYc Scale on X-Y planeArbitraryDirection Scale in arbitrary directionArbitraryPlane Scale on arbitrary plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-