StudioXformBuilderAdvancedMethodType Enumeration

NXOpen.Features.StudioXformBuilder.AdvancedMethodType is an alias for NXOpen.Features.StudioXformBuilderAdvancedMethodType

class NXOpen.Features.StudioXformBuilderAdvancedMethodType

Bases: object

Represents the advanced method type

Enum Members

Enum Member Enum Member Description
ChangeDegree
Change degree
Falloff
Fall off
ProportionalMovement
Proportional movement
KeepContinuity
Keep continuity
LockRegion
Lock region
InsertKnot
Insert knot
AdvanceOff
Turn off advanced methods
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.