StudioXformBuilderTypes Enumeration

NXOpen.Features.StudioXformBuilder.Types is an alias for NXOpen.Features.StudioXformBuilderTypes

class NXOpen.Features.StudioXformBuilderTypes

Bases: object

Represents the Xform type

Enum Members

Enum Member Enum Member Description
Translate
Translate type of Xform
Rotate
Rotate type of Xform
Scale
Scale type of Xform
TranslateNormalToFaceOrCurve
Along normal type of Xform
TranlsateAlongControlPolygon
Along polygon type of Xform
PlanarizeRowOfPoles
Planarize type of Xform
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.