StudioXformBuilderTranslationDirectionType Enumeration

NXOpen.Features.StudioXformBuilder.TranslationDirectionType is an alias for NXOpen.Features.StudioXformBuilderTranslationDirectionType

class NXOpen.Features.StudioXformBuilderTranslationDirectionType

Bases: object

Represents the translation direction type

Enum Members

Enum Member Enum Member Description
Xc
Translate in X direction
Yc
Translate in Y direction
Zc
Translate in Z direction
YcZc
Translate on Y-Z plane
XcZc
Translate on X-Z plane
XcYc
Translate on X-Y plane
ArbitraryDirection
Translate in arbitrary direction
ArbitraryPlane
Translate on arbitrary plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.