StudioXformBuilderRotatingPivotType Enumeration¶
NXOpen.Features.StudioXformBuilder.RotatingPivotType is an alias for NXOpen.Features.StudioXformBuilderRotatingPivotType
-
class
NXOpen.Features.
StudioXformBuilderRotatingPivotType
¶ Bases:
object
Represents the rotating pivot type
Enum Members
Enum Member Enum Member Description AboutObjectCenter Rotate pivot at the object centerAboutSelectedObject Rotate pivot at the selected objectAboutPoint Rotate pivot at a point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-