StudioXformBuilderPlanarizeMethodType Enumeration

NXOpen.Features.StudioXformBuilder.PlanarizeMethodType is an alias for NXOpen.Features.StudioXformBuilderPlanarizeMethodType

class NXOpen.Features.StudioXformBuilderPlanarizeMethodType

Bases: object

Represents the planarize method type

Enum Members

Enum Member Enum Member Description
AtPlaneLocation
planarize at plane location
AtPoleLocation
planarize at pole location
OnABestFitPlane
planarize at a best fit plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.