StudioXformBuilderRotationDirectionType Enumeration¶
NXOpen.Features.StudioXformBuilder.RotationDirectionType is an alias for NXOpen.Features.StudioXformBuilderRotationDirectionType
-
class
NXOpen.Features.
StudioXformBuilderRotationDirectionType
¶ Bases:
object
Represents the rotation direction type
Enum Members
Enum Member Enum Member Description Xc Rotate in X directionYc Rotate in Y directionZc Rotate in Z directionArbitraryDirection Rotate in arbitrary directionArbitraryPlane Rotate on arbitrary plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-