StudioXformBuilderFeatureType Enumeration

NXOpen.Features.StudioXformBuilder.FeatureType is an alias for NXOpen.Features.StudioXformBuilderFeatureType

class NXOpen.Features.StudioXformBuilderFeatureType

Bases: object

Represents the feature type

Enum Members

Enum Member Enum Member Description
Relative
Relative feature type of Xform
Absolute
Absolute feature type of Xform
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.