NXOpen.PDM.AlternateIdManager |
This class is responsible for setting and getting NX Manager database attribute. |
NXOpen.PDM.AttributeGroup |
Represents an attribute group. |
NXOpen.PDM.AttributeGroupCollection |
Represents a collection of attribute group objects. |
NXOpen.PDM.AttributeGroupDescription |
Represents an attribute group type. |
NXOpen.PDM.AttributeGroupDescriptionCollection |
Represents a collection of attribute group description objects. |
NXOpen.PDM.AttributeGroupReviseBuilder |
Represents an attribute group revise builder. |
NXOpen.PDM.CAEFileContainer |
This class is a File Container class for uploading JT files created by NX CAE Post Processing to Teamcenter. |
NXOpen.PDM.CaeCloneManager |
This class is used for executing CAE Clone on a Simulation File or a FeModel File. |
NXOpen.PDM.ConfigurationContextBuilder |
Represents a NXOpen.PDM.ConfigurationContextBuilder builder |
NXOpen.PDM.ConfigurationManager |
Represents Configuration Manager |
NXOpen.PDM.DatabaseAttributeManager |
This class is responsible for setting and getting NX Manager database attribute. |
NXOpen.PDM.DesignElementRevision |
Represents the design element revision in the database. |
NXOpen.PDM.DesignFeatureRevision |
Represents the design feature revision in the database. |
NXOpen.PDM.DesignSubordinateRevision |
Represents the design subordinate revision in the database. |
NXOpen.PDM.EffectivityAttributePropertiesBuilder |
Represents an NXOpen.PDM.EffectivityAttributePropertiesBuilder to be used for creating effectivity attributes. |
NXOpen.PDM.EffectivityTableBuilder |
Represents a builder class for effectivity configuration. |
NXOpen.PDM.EffectivityTableRow |
Represents the class that contains effectivity parameters. |
NXOpen.PDM.FileManagement |
This class is responsible for Teamcenter file management related activities. |
NXOpen.PDM.GenericObjectAttributeHolder |
Represents the class that contains database business logic or pre-creation information for the objects. |
NXOpen.PDM.IAttributeGroupOwner |
An interface class for objects that own attribute groups. |
NXOpen.PDM.ListOfValues |
Represents list of values to be used in search query |
NXOpen.PDM.LogicalObject |
Represents the class that contains database business logic or pre-creation information for the objects. |
NXOpen.PDM.ModelElementRevision |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
NXOpen.PDM.NativePartLogicalObject |
Represents the class that contains information for the objects participating in import operation. |
NXOpen.PDM.ObjectCreateBuilder |
Represents a builder class that perofrms create operation |
NXOpen.PDM.OperationErrors |
Represents Operation Errors to be returned in TCIN related operations |
NXOpen.PDM.PartBuilder |
This class serves as the base class for NX Manager part builders. |
NXOpen.PDM.PartCreationObject |
This class is a proxy for a to-be-created part prior to the part being created. |
NXOpen.PDM.PartCreationObjectAttributePropertiesBuilder |
Represents an NXOpen.PDM.PartCreationObjectAttributePropertiesBuilder . |
NXOpen.PDM.PartFromPartBuilder |
This class provides the methods necessary to create a new part in NX Manager from an existing part. |
NXOpen.PDM.PartFromTemplateBuilder |
This class provides the methods necessary to create a new part in NX Manager from a template part. |
NXOpen.PDM.PartManager |
This class contains methods to create and manage parts in NX Manager mode. |
NXOpen.PDM.PartOperationAttributePropertiesBuilder |
Represents an NXOpen.PDM.PartOperationAttributePropertiesBuilder to be used for creating attributes in part operation. |
NXOpen.PDM.PartOperationBuilder |
Represents a builder class that performs various design element operations. |
NXOpen.PDM.PartOperationCopyBuilder |
Represents a builder class that performs various Save As operations. |
NXOpen.PDM.PartOperationCreateBuilder |
Represents a builder class that performs Create operations |
NXOpen.PDM.PartOperationImportBuilder |
Represents a builder class that performs Create operations |
NXOpen.PDM.PartOperationImportCallbackData |
JA interface for PartOperationImportCallbackData object |
NXOpen.PDM.PartOperationImportObserver |
This class is responsible for invoking registered callbacks at different stages in import operation. |
NXOpen.PDM.PartOperationMakeUniqueBuilder |
Represents a NXOpen.PDM.PartOperationMakeUniqueBuilder builder |
NXOpen.PDM.PartOperationValidationPropertiesBuilder |
Represents an NXOpen.PDM.PartOperationValidationPropertiesBuilder to be used for overriding the default validation parameters for a part in import operation. |
NXOpen.PDM.PdmNavigatorNode |
Represents a PdmNavigatorNode |
NXOpen.PDM.PdmPart |
This class serves as a gateway to part-specific tools for NX Manager mode. |
NXOpen.PDM.PdmSearch |
Represents search query |
NXOpen.PDM.PdmSearchManager |
Represents search manager class |
NXOpen.PDM.PdmSession |
Represents the NX Manager session |
NXOpen.PDM.PendingComponentsManager |
This class is used for managing a part’s pending components, that is, those that have been added within Teamcenter but are not yet present in NX. |
NXOpen.PDM.PersistentSettings |
Persistently held settings for a Teamcenter user account. |
NXOpen.PDM.RequirementUtils |
Collection of PDM utility methods |
NXOpen.PDM.SearchResult |
Represents search query |
NXOpen.PDM.SessionSettings |
Values for the settings that affect the current Teamcenter session. |
NXOpen.PDM.SoaQuery |
Represents search soa query to perform Teamcenter search |
NXOpen.PDM.TracelinkQuery |
Represents the Trace link query |
NXOpen.PDM.VariantConfigurationBuilder |
Represents a builder class that performs variant rule configuration. |