PartOperationImportBuilder Class¶
-
class
NXOpen.PDM.
PartOperationImportBuilder
¶ Bases:
NXOpen.PDM.PartOperationBuilder
Represents a builder class that performs Create operations
To create a new instance of this class, use
NXOpen.PDM.PdmSession.CreateImportOperationBuilder
Default values.
Property Value ConversionType AsID DefaultAction Overwrite IncludeComponentParts 1 IncludeDependentParts 0 NumberingSource PartIDGenerator ValidationAbortImportOnFail 0 ValidationMode Off ValidationRuleSetBrowseOption Native ValidationTreatOutdatedAsPass 0 ValidationTreatWarningAsPass 1 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AddDfaMixins | Returns or sets the add dfa mixins |
AssociatedFilesRootDirectory | Returns or sets the associated files root directory |
ConversionType | Returns or sets the conversion type |
DefaultAction | Returns or sets the default action |
DefaultDescription | Returns or sets the default description |
DefaultDestinationFolder | Returns or sets the default destination folder string for the part being created . |
DefaultItemType | Returns or sets the default item type |
DefaultName | Returns or sets the default name |
DefaultOwningGroup | Returns or sets the default owning group |
DefaultOwningUser | Returns or sets the default owning user |
DependentFileSaveAsOption | Returns or sets the Dependent files Save As option. |
IncludeComponentParts | Returns or sets the include component parts |
IncludeDependentParts | Returns or sets the include dependent parts |
NumberAttr | Returns or sets the number attr |
NumberingSource | Returns or sets the numbering source |
OutputLogFile | Returns or sets the output log file |
PrefixStr | Returns or sets the prefix str |
ProductInterfaces | Returns or sets the product interfaces |
PublishOptionalInfo | Returns or sets the optional information publishing |
ReplaceAllComponents | Returns or sets the replace all components. |
ReplaceWithStr | Returns or sets the replace with str |
RevisionAttr | Returns or sets the revision attr |
StringToReplace | Returns or sets the string to replace |
SuffixStr | Returns or sets the suffix str |
SyncArrangements | Returns or sets the sync arrangements |
Tag | Returns the Tag for this object. |
ValidationAbortImportOnFail | Returns or sets the validation abort import on fail |
ValidationMode | Returns or sets the validation mode |
ValidationRuleSetBrowseOption | Returns or sets the validation rule set browse option |
ValidationRuleSetFile | Returns or sets the validation rule set file |
ValidationTreatOutdatedAsPass | Returns or sets the validation treat outdated as pass |
ValidationTreatWarningAsPass | Returns or sets the validation treat warning as pass |
Methods¶
Method | Description |
---|---|
AddParts | Add parts to import |
AddPartsFromFolder | Add parts to import from selected folder |
AddPartsUsingLogFile | Add parts using log file either clone log file or import log file |
AddRelatedPartToOperate | Add related part to the part undergoing an operation. |
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
Commit | Commits any edits that have been applied to the builder. |
CreateLogicalObjects | Creates the pre-creation objects for the parts |
CreateNonMasterListForLogicalObject | Create NonMaster list for the selected logical Object |
CreateSpecificationsForLogicalObjects | Create new specifications for Logical Objects |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditNonMasterName | Sets the name the non-master part will get saved as. |
ExecuteDryRun | Execute the dry run |
GetAlternateIDManager | Create an instance of a NXOpen.PDM.AlternateIdManager class that will be used to create alternate ID information while creating the new part. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDefaultProjectInformation | Get default projects information |
GetDfaFiles | Get the dfa files |
GetDialogOperation | Returns the dialog operation Applicable only for operation types PartOperationBuilderOperationType.SaveAs and PartOperationBuilderOperationType.Revise @return |
GetLogicalObjectForPart | Gets the known logical object for the given part filename. |
GetNonMasterCopyOption | Get the nonmasters saveAs option for given logical object. |
GetNonMasterList | Gets NonMaster list for the given logical Object @return Non-master part file names |
GetObject | Returns the object currently being edited by this builder. |
GetOperationFailures | Returns part operation failures @return |
GetUpdatedLogicalObjects | Gets the updated logical object objects for the parts after item type, relation type or master part for nonmaster is set or changed. |
IsNonMasterBeingCopied | Returns whether or not the non master part specified for the given :py:class:`NXOpen.PDM.LogicalObject`will actually get saved during the save as operation. |
RemoveDfaFile | Remove the dfa file |
ResetAttributes | Clear all attributes from the selected logical objects |
SetDefaultProjectInformation | Set default projects information |
SetDfaFiles | Set the dfa files |
SetDialogOperation | Sets the dialog operation. |
SetExistingPartAttributes | Apply existing item attributes |
SetNonMasterSaveAsOption | Set the nonmasters saveAs option for given logical object |
SetSelectedNonMasterToSaveAs | Sets whether or not the non-master part specified will actually get saved during the save as operation. |
SetSelectedParts | Sets the selected parts. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateLogicalObjectsToCommit | Validates NXOpen.PDM.LogicalObject objects with this builder and udpates the operation failuers. |
Enumerations¶
PartOperationImportBuilderConversionRule Enumeration | This enum is used to specify the conversion rule for <ja_type>JA_PART_OPERATION_IMPORT_BUILDER_NumberingSourceOption_OSFilename</ja_type>. |
PartOperationImportBuilderExistingPartAction Enumeration | This enum is used to specify the default action for import. |
PartOperationImportBuilderNumberingSourceOption Enumeration | This enum is used to specify the default behavior for auto assign. |
PartOperationImportBuilderValidation Enumeration | This enum is used to specify the validation mode. |
PartOperationImportBuilderValidationRuleSetFileBrowseOption Enumeration | This enum is used to specify the option to browse the validation rule set file from. |
Property Detail¶
AddDfaMixins¶
-
PartOperationImportBuilder.
AddDfaMixins
¶ Returns or sets the add dfa mixins
-------------------------------------
Getter Method
Signature
AddDfaMixins()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddDfaMixins(addDfaMixins)
Parameters: addDfaMixins (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
AssociatedFilesRootDirectory¶
-
PartOperationImportBuilder.
AssociatedFilesRootDirectory
¶ Returns or sets the associated files root directory
-------------------------------------
Getter Method
Signature
AssociatedFilesRootDirectory()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssociatedFilesRootDirectory(foldername)
Parameters: foldername (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ConversionType¶
-
PartOperationImportBuilder.
ConversionType
¶ Returns or sets the conversion type
-------------------------------------
Getter Method
Signature
ConversionType()
Returns: Return type: NXOpen.PDM.PartOperationImportBuilderConversionRule
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConversionType(conversionType)
Parameters: conversionType ( NXOpen.PDM.PartOperationImportBuilderConversionRule
) –New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DefaultAction¶
-
PartOperationImportBuilder.
DefaultAction
¶ Returns or sets the default action
-------------------------------------
Getter Method
Signature
DefaultAction()
Returns: Return type: NXOpen.PDM.PartOperationImportBuilderExistingPartAction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultAction(defaultAction)
Parameters: defaultAction ( NXOpen.PDM.PartOperationImportBuilderExistingPartAction
) –New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DefaultDescription¶
-
PartOperationImportBuilder.
DefaultDescription
¶ Returns or sets the default description
-------------------------------------
Getter Method
Signature
DefaultDescription()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultDescription(defaultDescription)
Parameters: defaultDescription (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DefaultItemType¶
-
PartOperationImportBuilder.
DefaultItemType
¶ Returns or sets the default item type
-------------------------------------
Getter Method
Signature
DefaultItemType()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultItemType(defaultItemType)
Parameters: defaultItemType (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DefaultName¶
-
PartOperationImportBuilder.
DefaultName
¶ Returns or sets the default name
-------------------------------------
Getter Method
Signature
DefaultName()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultName(defaultName)
Parameters: defaultName (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DefaultOwningGroup¶
-
PartOperationImportBuilder.
DefaultOwningGroup
¶ Returns or sets the default owning group
-------------------------------------
Getter Method
Signature
DefaultOwningGroup()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultOwningGroup(defaultOwningGroup)
Parameters: defaultOwningGroup (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DefaultOwningUser¶
-
PartOperationImportBuilder.
DefaultOwningUser
¶ Returns or sets the default owning user
-------------------------------------
Getter Method
Signature
DefaultOwningUser()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultOwningUser(defaultOwningUser)
Parameters: defaultOwningUser (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IncludeComponentParts¶
-
PartOperationImportBuilder.
IncludeComponentParts
¶ Returns or sets the include component parts
-------------------------------------
Getter Method
Signature
IncludeComponentParts()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeComponentParts(includeComponentParts)
Parameters: includeComponentParts (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IncludeDependentParts¶
-
PartOperationImportBuilder.
IncludeDependentParts
¶ Returns or sets the include dependent parts
-------------------------------------
Getter Method
Signature
IncludeDependentParts()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeDependentParts(includeDependentParts)
Parameters: includeDependentParts (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
NumberAttr¶
-
PartOperationImportBuilder.
NumberAttr
¶ Returns or sets the number attr
-------------------------------------
Getter Method
Signature
NumberAttr()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberAttr(numberAttr)
Parameters: numberAttr (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
NumberingSource¶
-
PartOperationImportBuilder.
NumberingSource
¶ Returns or sets the numbering source
-------------------------------------
Getter Method
Signature
NumberingSource()
Returns: Return type: NXOpen.PDM.PartOperationImportBuilderNumberingSourceOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberingSource(numberingSource)
Parameters: numberingSource ( NXOpen.PDM.PartOperationImportBuilderNumberingSourceOption
) –New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
OutputLogFile¶
-
PartOperationImportBuilder.
OutputLogFile
¶ Returns or sets the output log file
-------------------------------------
Getter Method
Signature
OutputLogFile()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputLogFile(filename)
Parameters: filename (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
PrefixStr¶
-
PartOperationImportBuilder.
PrefixStr
¶ Returns or sets the prefix str
-------------------------------------
Getter Method
Signature
PrefixStr()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrefixStr(prefixStr)
Parameters: prefixStr (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ProductInterfaces¶
-
PartOperationImportBuilder.
ProductInterfaces
¶ Returns or sets the product interfaces
-------------------------------------
Getter Method
Signature
ProductInterfaces()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProductInterfaces(productInterfaces)
Parameters: productInterfaces (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
PublishOptionalInfo¶
-
PartOperationImportBuilder.
PublishOptionalInfo
¶ Returns or sets the optional information publishing
-------------------------------------
Getter Method
Signature
PublishOptionalInfo()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PublishOptionalInfo(publishOptionalInfo)
Parameters: publishOptionalInfo (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ReplaceWithStr¶
-
PartOperationImportBuilder.
ReplaceWithStr
¶ Returns or sets the replace with str
-------------------------------------
Getter Method
Signature
ReplaceWithStr()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReplaceWithStr(replaceWithStr)
Parameters: replaceWithStr (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
RevisionAttr¶
-
PartOperationImportBuilder.
RevisionAttr
¶ Returns or sets the revision attr
-------------------------------------
Getter Method
Signature
RevisionAttr()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RevisionAttr(revisionAttr)
Parameters: revisionAttr (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
StringToReplace¶
-
PartOperationImportBuilder.
StringToReplace
¶ Returns or sets the string to replace
-------------------------------------
Getter Method
Signature
StringToReplace()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringToReplace(stringToReplace)
Parameters: stringToReplace (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SuffixStr¶
-
PartOperationImportBuilder.
SuffixStr
¶ Returns or sets the suffix str
-------------------------------------
Getter Method
Signature
SuffixStr()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SuffixStr(suffixStr)
Parameters: suffixStr (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SyncArrangements¶
-
PartOperationImportBuilder.
SyncArrangements
¶ Returns or sets the sync arrangements
-------------------------------------
Getter Method
Signature
SyncArrangements()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SyncArrangements(syncArrangements)
Parameters: syncArrangements (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ValidationAbortImportOnFail¶
-
PartOperationImportBuilder.
ValidationAbortImportOnFail
¶ Returns or sets the validation abort import on fail
-------------------------------------
Getter Method
Signature
ValidationAbortImportOnFail()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidationAbortImportOnFail(validationAbortImportOnFail)
Parameters: validationAbortImportOnFail (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ValidationMode¶
-
PartOperationImportBuilder.
ValidationMode
¶ Returns or sets the validation mode
-------------------------------------
Getter Method
Signature
ValidationMode()
Returns: Return type: NXOpen.PDM.PartOperationImportBuilderValidation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidationMode(validationMode)
Parameters: validationMode ( NXOpen.PDM.PartOperationImportBuilderValidation
) –New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ValidationRuleSetBrowseOption¶
-
PartOperationImportBuilder.
ValidationRuleSetBrowseOption
¶ Returns or sets the validation rule set browse option
-------------------------------------
Getter Method
Signature
ValidationRuleSetBrowseOption()
Returns: Return type: NXOpen.PDM.PartOperationImportBuilderValidationRuleSetFileBrowseOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidationRuleSetBrowseOption(validationRuleSetBrowseOption)
Parameters: validationRuleSetBrowseOption ( NXOpen.PDM.PartOperationImportBuilderValidationRuleSetFileBrowseOption
) –New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ValidationRuleSetFile¶
-
PartOperationImportBuilder.
ValidationRuleSetFile
¶ Returns or sets the validation rule set file
-------------------------------------
Getter Method
Signature
ValidationRuleSetFile()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidationRuleSetFile(filename)
Parameters: filename (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ValidationTreatOutdatedAsPass¶
-
PartOperationImportBuilder.
ValidationTreatOutdatedAsPass
¶ Returns or sets the validation treat outdated as pass
-------------------------------------
Getter Method
Signature
ValidationTreatOutdatedAsPass()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidationTreatOutdatedAsPass(validationTreatOutdatedAsPass)
Parameters: validationTreatOutdatedAsPass (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ValidationTreatWarningAsPass¶
-
PartOperationImportBuilder.
ValidationTreatWarningAsPass
¶ Returns or sets the validation treat warning as pass
-------------------------------------
Getter Method
Signature
ValidationTreatWarningAsPass()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidationTreatWarningAsPass(validationTreatWarningAsPass)
Parameters: validationTreatWarningAsPass (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
AddParts¶
-
PartOperationImportBuilder.
AddParts
¶ Add parts to import
Signature
AddParts(parts)
Parameters: parts (list of str) – Returns: Return type: list of str New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
AddPartsFromFolder¶
-
PartOperationImportBuilder.
AddPartsFromFolder
¶ Add parts to import from selected folder
Signature
AddPartsFromFolder(folderPath)
Parameters: folderPath (str) – Returns: Return type: list of str New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
AddPartsUsingLogFile¶
-
PartOperationImportBuilder.
AddPartsUsingLogFile
¶ Add parts using log file either clone log file or import log file
Signature
AddPartsUsingLogFile(logFilePath)
Parameters: logFilePath (str) – Returns: Return type: list of str New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
AutoAssignAttributes¶
-
PartOperationImportBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
ExecuteDryRun¶
-
PartOperationImportBuilder.
ExecuteDryRun
¶ Execute the dry run
Signature
ExecuteDryRun()
New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetDefaultProjectInformation¶
-
PartOperationImportBuilder.
GetDefaultProjectInformation
¶ Get default projects information
Signature
GetDefaultProjectInformation()
Returns: a tuple Return type: A tuple consisting of (projectNames, assignmentStates). projectNames is a list of str. names of the projects assignmentStates is a list of NXOpen.SessionProjectAssignmentState
. assignment statesNew in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
GetDfaFiles¶
-
PartOperationImportBuilder.
GetDfaFiles
¶ Get the dfa files
Signature
GetDfaFiles()
Returns: Return type: list of str New in version NX10.0.0.
License requirements: None.
GetLogicalObjectForPart¶
-
PartOperationImportBuilder.
GetLogicalObjectForPart
¶ Gets the known logical object for the given part filename.
Signature
GetLogicalObjectForPart(partFilename)
Parameters: partFilename (str) – Returns: Return type: NXOpen.PDM.LogicalObject
New in version NX10.0.0.
License requirements: None.
GetUpdatedLogicalObjects¶
-
PartOperationImportBuilder.
GetUpdatedLogicalObjects
¶ Gets the updated logical object objects for the parts after item type, relation type or master part for nonmaster is set or changed.
Signature
GetUpdatedLogicalObjects()
Returns: Return type: list of NXOpen.PDM.LogicalObject
New in version NX10.0.0.
License requirements: None.
RemoveDfaFile¶
-
PartOperationImportBuilder.
RemoveDfaFile
¶ Remove the dfa file
Signature
RemoveDfaFile(filename)
Parameters: filename (str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
ResetAttributes¶
-
PartOperationImportBuilder.
ResetAttributes
¶ Clear all attributes from the selected logical objects
Signature
ResetAttributes(logicalObjects)
Parameters: logicalObjects (list of NXOpen.PDM.LogicalObject
) –New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SetDefaultProjectInformation¶
-
PartOperationImportBuilder.
SetDefaultProjectInformation
¶ Set default projects information
Signature
SetDefaultProjectInformation(projectNames, assignmentStates)
Parameters: - projectNames (list of str) – names of the projects to assign NOTE: The full Unicode character set is not supported for this parameter.
- assignmentStates (list of
NXOpen.SessionProjectAssignmentState
) – assignment states
New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SetDfaFiles¶
-
PartOperationImportBuilder.
SetDfaFiles
¶ Set the dfa files
Signature
SetDfaFiles(dfaFiles)
Parameters: dfaFiles (list of str) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SetExistingPartAttributes¶
-
PartOperationImportBuilder.
SetExistingPartAttributes
¶ Apply existing item attributes
Signature
SetExistingPartAttributes(logicalObject, cliSpec)
Parameters: - logicalObject (
NXOpen.PDM.LogicalObject
) – - cliSpec (str) –
New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- logicalObject (
Validate¶
-
PartOperationImportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.