SoaQuery Class¶
-
class
NXOpen.PDM.
SoaQuery
¶ Bases:
NXOpen.TransientObject
Represents search soa query to perform Teamcenter search
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
AddFieldDescription | Add the field description to create an SOA query |
Dispose | Frees the object from memory. |
Method Detail¶
AddFieldDescription¶
-
SoaQuery.
AddFieldDescription
¶ Add the field description to create an SOA query
Signature
AddFieldDescription(searchVar, type, name, attrName, defaultValue, logicalOperation, mathOperation, lov)
Parameters: - searchVar (
NXOpen.PDM.PdmSearch
) – pdm search structure - type (
NXOpen.PDM.PdmSoaqueryNxmgrfielddatatype
) – search field data type - name (str) – name of search NOTE: The full Unicode character set is not supported for this parameter.
- attrName (str) – search attribute name NOTE: The full Unicode character set is not supported for this parameter.
- defaultValue (str) – default value NOTE: The full Unicode character set is not supported for this parameter.
- logicalOperation (str) – logical operation for search criteria NOTE: The full Unicode character set is not supported for this parameter.
- mathOperation (str) – math operation for search criteria NOTE: The full Unicode character set is not supported for this parameter.
- lov (
NXOpen.PDM.ListOfValues
) – List of values
New in version NX6.0.0.
Deprecated since version NX8.0.0: It’s not needed in any context of search based on queries.
License requirements: None.
- searchVar (