PartBuilderPartFileNameData_Struct Struct¶
NXOpen.PDM.PartBuilder.PartFileNameData is an alias for NXOpen.PDM.PartBuilderPartFileNameData_Struct
-
class
NXOpen.PDM.
PartBuilderPartFileNameData_Struct
¶ Bases:
object
Contains part file name information
Fields¶
Field | Description |
---|---|
PartFileName | Part file name |
PartFileNameModifiable | False if part file name is not modifiable |
PartFileName¶
-
PartBuilderPartFileNameData_Struct.
PartFileName
¶ Part file name
-------------------------------------
Getter Method Signature
PartFileName()
Returns: Return type: str -------------------------------------
Setter Method
Signature
PartFileName(value)
Parameters: value (str) –
PartFileNameModifiable¶
-
PartBuilderPartFileNameData_Struct.
PartFileNameModifiable
¶ False if part file name is not modifiable
-------------------------------------
Getter Method Signature
PartFileNameModifiable()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
PartFileNameModifiable(value)
Parameters: value (bool) –