AttributeGroupCollection Class¶
-
class
NXOpen.PDM.
AttributeGroupCollection
¶ Bases:
object
Represents a collection of attribute group objects.
A smaller list of attribute groups can be retrieved by using the method
NXOpen.PDM.IAttributeGroupOwner.GetAttributeGroups
for classes that implement theNXOpen.PDM.IAttributeGroupOwner
interface. To obtain an instance of this class, refer toNXOpen.CollaborativeDesign
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.PDM.AttributeGroup with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
AttributeGroupCollection.
FindObject
¶ Finds the
NXOpen.PDM.AttributeGroup
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier to be found Returns: AttributeGroup found, or null if no such attribute group exists. Return type: NXOpen.PDM.AttributeGroup
New in version NX9.0.0.
License requirements: None.