SearchResult Class¶
-
class
NXOpen.PDM.
SearchResult
¶ Bases:
NXOpen.TransientObject
Represents search query
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetResultItemIds | Gets a list of the item_ids from the search result. |
GetResultMfkIds | Gets a list of the Multifield Keys from the search results. |
GetResultObjectNames | Gets a list of the object names from the search result @return array of object names |
GetResultObjectTypes | Gets a list of the object types from the search result @return array of object types |
Method Detail¶
Dispose¶
-
SearchResult.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetResultItemIds¶
-
SearchResult.
GetResultItemIds
¶ Gets a list of the item_ids from the search result.
If Multifield Key environment is enabled, then use Multifield key function
PDM.SearchResult.GetResultMfkIds
, as this function may return us duplicate item ids if the corresponding parts belong to different domains.Signature
GetResultItemIds()
Returns: array of item_ids Return type: list of str New in version NX8.5.0.
Deprecated since version NX10.0.0: Use
PDM.SearchResult.GetResultMfkIds
instead.License requirements: None.
GetResultMfkIds¶
-
SearchResult.
GetResultMfkIds
¶ Gets a list of the Multifield Keys from the search results.
If Multifield Key environment is enabled then always use this function Multifield Key: e.g. %#MFK#%,=item_id=001, object_type=SupplierPart, supplier_code=x
Signature
GetResultMfkIds()
Returns: array of mfk_ids Return type: list of str New in version NX10.0.0.
License requirements: None.