PartOperationCopyBuilderCopyDependentFiles Enumeration¶
NXOpen.PDM.PartOperationCopyBuilder.CopyDependentFiles is an alias for NXOpen.PDM.PartOperationCopyBuilderCopyDependentFiles
-
class
NXOpen.PDM.
PartOperationCopyBuilderCopyDependentFiles
¶ Bases:
object
This enum is used to specify which dependent files should be copied to new part during the save as operation.
New in version NX10.0.0.
Enum Members
Enum Member Enum Member Description All save all during save asNone save none during save as-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-