PartOperationMakeUniqueBuilder Class¶
-
class
NXOpen.PDM.
PartOperationMakeUniqueBuilder
¶ Bases:
NXOpen.PDM.PartOperationCopyBuilder
Represents a
NXOpen.PDM.PartOperationMakeUniqueBuilder
builderTo create a new instance of this class, use
NXOpen.PDM.PdmSession.CreateMakeUniqueOperationBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DefaultDestinationFolder | Returns or sets the default destination folder string for the part being created . |
DependentFileSaveAsOption | Returns or sets the Dependent files Save As option. |
DependentFilesToCopyOption | Returns or sets the Dependent files Save As option. |
ReplaceAllComponents | Returns or sets the replace all components. |
ReplaceAllComponentsInSession | Returns or sets the replace all components. |
SelectedComponents | Returns the selected components to be made unique are returned. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddRelatedPartToOperate | Add related part to the part undergoing an operation. |
AddRelatedPartsToCopy | Add related part to the part undergoing an operation. |
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
Commit | Commits any edits that have been applied to the builder. |
CreateLogicalObjects | Creates the pre-creation objects for the parts |
CreateNonMasterListForCopyLogicalObject | Create NonMaster list for the selected logical Object |
CreateNonMasterListForLogicalObject | Create NonMaster list for the selected logical Object |
CreateSpecificationsForLogicalObjects | Create new specifications for Logical Objects |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditNonMasterName | Sets the name the non-master part will get saved as. |
EditNonMasterToCopyName | Sets the name the non-master part will get saved as. |
GetAlternateIDManager | Create an instance of a NXOpen.PDM.AlternateIdManager class that will be used to create alternate ID information while creating the new part. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCopyNonMasterPartsOption | Get the nonmasters saveAs option for given logical object. |
GetDialogOperation | Returns the dialog operation Applicable only for operation types PartOperationBuilderOperationType.SaveAs and PartOperationBuilderOperationType.Revise @return |
GetNonMasterCopyOption | Get the nonmasters saveAs option for given logical object. |
GetNonMasterList | Gets NonMaster list for the given logical Object @return Non-master part file names |
GetNonMasterListForCopyLogicalObject | Gets NonMaster list for the given logical Object @return Non-master part file names |
GetObject | Returns the object currently being edited by this builder. |
GetOperationFailures | Returns part operation failures @return |
GetOperationSubType | Returns the NXOpen.PDM.PartOperationCopyBuilderOperationSubType for Create. |
IsNonMasterBeingCopied | Returns whether or not the non master part specified for the given :py:class:`NXOpen.PDM.LogicalObject`will actually get saved during the save as operation. |
IsNonMasterForLogicalObjectBeingCopied | Returns whether or not the non-master part specified for the given :py:class:`NXOpen.PDM.LogicalObject`will actually get saved during the save as operation. |
SetCopyNonMasterPartsOption | Set the nonmasters saveAs option for given logical object. |
SetDialogOperation | Sets the dialog operation. |
SetNonMasterSaveAsOption | Set the nonmasters saveAs option for given logical object |
SetOperationSubType | Sets the NXOpen.PDM.PartOperationCopyBuilderOperationSubType for Create. |
SetSelectedNonMasterToCopy | Sets whether or not the non-master part specified will actually get saved during the save as operation. |
SetSelectedNonMasterToSaveAs | Sets whether or not the non-master part specified will actually get saved during the save as operation. |
SetSelectedParts | Sets the selected parts. |
SetSelectedPartsToCopy | Sets the selected parts. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateLogicalObjectsToCommit | Validates NXOpen.PDM.LogicalObject objects with this builder and udpates the operation failuers. |
Property Detail¶
SelectedComponents¶
-
PartOperationMakeUniqueBuilder.
SelectedComponents
¶ Returns the selected components to be made unique are returned.
-------------------------------------
Getter Method
Signature
SelectedComponents()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
Method Detail¶
AutoAssignAttributes¶
-
PartOperationMakeUniqueBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
Validate¶
-
PartOperationMakeUniqueBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.