ObjectCreateBuilder Class¶
-
class
NXOpen.PDM.
ObjectCreateBuilder
¶ Bases:
NXOpen.Builder
,NXOpen.IAttributeSourceObjectBuilder
Represents a builder class that perofrms create operation
To create a new instance of this class, use
NXOpen.PDM.PdmSession.CreateObjectCreateBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DefaultDestinationFolder | Returns or sets the default destination folder string for the object being created. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
Commit | Commits any edits that have been applied to the builder. |
CreateLogicalObjects | Creates Pre-Creation LogicalObjects |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAttributeHolderObjects | Returns an array of AttributeHolderObjects created as part of commit. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetTypes | Set Types for which AttributeHolderObject needs to be created. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DefaultDestinationFolder¶
-
ObjectCreateBuilder.
DefaultDestinationFolder
¶ Returns or sets the default destination folder string for the object being created.
The default destination folder string can be <username>:<folder>:<folder>, or :<folder>:<folder> means username is optional. In case of :<folder>:<folder>, the first : indicates Home, for example, :Newstuff, is the Newstuff folder in current user’s Home container.
-------------------------------------
Getter Method
Signature
DefaultDestinationFolder()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultDestinationFolder(defaultDestinationFolder)
Parameters: defaultDestinationFolder (str) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
AutoAssignAttributes¶
-
ObjectCreateBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
CreateLogicalObjects¶
-
ObjectCreateBuilder.
CreateLogicalObjects
¶ Creates Pre-Creation LogicalObjects
Signature
CreateLogicalObjects()
Returns: Return type: list of NXOpen.PDM.LogicalObject
New in version NX10.0.0.
License requirements: None.
GetAttributeHolderObjects¶
-
ObjectCreateBuilder.
GetAttributeHolderObjects
¶ Returns an array of AttributeHolderObjects created as part of commit.
Signature
GetAttributeHolderObjects()
Returns: Return type: list of NXOpen.PDM.GenericObjectAttributeHolder
New in version NX10.0.0.
License requirements: None.
SetTypes¶
-
ObjectCreateBuilder.
SetTypes
¶ Set Types for which AttributeHolderObject needs to be created.
This method will remove all previously set types.
Signature
SetTypes(tcTypes, baseTCTypes)
Parameters: - tcTypes (list of str) –
- baseTCTypes (list of str) –
New in version NX10.0.0.
License requirements: None.
Validate¶
-
ObjectCreateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.